This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Single_cam application resolution

Part Number: TDA4VM


Hello,

I am new with vision_apps and I have a question about re-scaling in single_cam application.

I have a camera with a 1280x720 camera and a 1920x1080 monitor. When I run single_cam application (without LDC filter) I don't see the video in full-screen mode, but when I run it with LDC filter, I see the video in full-screen mode (pictures attached)

Output without LDC filter

Output with LDC filter

I would like to modify the application to show my image in full-screen mode but without LDC filter. I tried to read the code where LDC filter is applied but I couldn't identify where the image is resized.

I have read that up-scaling is not possible, but I don't know if technically is the same that showing an image in full-screen mode. And if both are the same, why I can see LDC image in full-screen?

I am currently using psdk-rtos-j721e-evm-08_00_00_12.

Thank you so much, regards!