This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64GPEVM: Ethernet Transmit Speed is Low

Part Number: TMDS64GPEVM

Hello,

I made iperf3 tests on TMDS64GPEVM. When I set TMDS64GPEVM as server and host pc as a client, I can see approx. 920Mbit/s speed but If I set TMDS64GPEVM as a client and host pc as server, I see 500-700Mbit/s speeds and the speed is not stable.

TMDS64GPEVM is connected on eth0 (DP83867).

 I'm using rt wic image from Processor SDK version 08.02.00.23 on SD card.

  • Hi,

    This documentation link is from the SDK guide. Could you please try the commands listed here to see if you are seeing the same numbers?

    Best Regards,

    Schuyler

  • Hi,

    Results of the tests:

    MIGRATED TCP STREAM TEST from 0.0.0.0 (0.0.0.0) port 0 AF_INET to 10.42.0.102 () port 0 AF_INET : histogram : interval
    Recv   Send    Send                          Utilization       Service Demand
    Socket Socket  Message  Elapsed              Send     Recv     Send    Recv
    Size   Size    Size     Time     Throughput  local    remote   local   remote
    bytes  bytes   bytes    secs.    10^6bits/s  % S      % S      us/KB   us/KB
    
    131072  16384  16384    60.00       554.19   70.88    1.52     20.955  3.606
    MIGRATED TCP MAERTS TEST from 0.0.0.0 (0.0.0.0) port 0 AF_INET to 10.42.0.102 () port 0 AF_INET : histogram : interval
    Recv   Send    Send                          Utilization       Service Demand
    Socket Socket  Message  Elapsed              Recv     Send     Recv    Send
    Size   Size    Size     Time     Throughput  local    remote   local   remote
    bytes  bytes   bytes    secs.    10^6bits/s  % S      % S      us/KB   us/KB
    
    131072  16384  16384    60.00       924.16   95.92    1.38     17.005  1.950