Hi team,
Here's an issue from the customer may need your help:
When using Port2 in 2G CPSW in MCU domain as an Ethernet entity and a port interconnect in 5G, the number of buffers configured in macl for transmit and receive is 48. After initialization is successful, the 2G side PORT1 sends a message. After sending more than the configured buffer, no further data can be transmitted. No free buffer is requested and the message can be received properly.
The array gEthTxCqRingMem cannot write data.
uint8 ArpData_VLAN3[32] =
{
0x00,0x03,0x08,06,0x00, 0x01, 0x08, 0x00, 0x06, 0x04, 0x00, 0x01, 0x00, 0x03, 0x19, 0x00, 0x00, 0x01,
0xa9, 0xfe, 0xfe, 0xab, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xa9, 0xfe, 0xab, 0xa8
};
uint8 MacDestUncastAddress[8] = {0xaa, 0xbb, 0xcc, 0xdd, 0xee, 0x06};
uint8 *TmpBuffPtr;
void Tx_EthFrame_VLAN3(void)
{
boolean Txstatus=0;
uint16 Tmp_Txlenghth1 = 32;
Global_TempUSage[1] = Eth_ProvideTxBuffer(0, 0, &TmpBuffIdx, &TmpBuffPtr, &Tmp_Txlenghth1);
ArpData[15] = gCnt++;
if(TmpBuffPtr != NULL_PTR)
{
TxBufferFill(TmpBuffPtr, Tmp_Txlenghth1, ArpData_VLAN3);
EthDemoRetVal[1] = Eth_Transmit(0, TmpBuffIdx, ETH_VLAN_PROTOCOL, Txstatus, Tmp_Txlenghth1, &MacDestUncastAddress[0]);
}
else
EthDemoRetVal[1] = 1;
}
#ifdef __cplusplus
extern "C" {
#endif
/* ========================================================================== */
/* Macros & Typedefs */
/* ========================================================================== */
/**
* \brief ETH Build Variant
* STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild
*/
#define ETH_PRE_COMPILE_VARIANT (STD_ON)
/** \brief Enable/disable SPI get version info API */
#define ETH_VERSION_INFO_API (STD_ON)
/** \brief Enable/disable Eth time sync related API */
#define ETH_GLOBALTIMESUPPORT_API (STD_OFF)
/** \brief Enable/Disable Development Error Detection */
#define ETH_DEV_ERROR_DETECT (STD_OFF)
/** \brief Enable/disable Eth get counter values API */
#define ETH_GET_COUNTER_VALUES_API (STD_ON)
/** \brief Enable/disable Eth get RX stats count API */
#define ETH_GET_RX_STATS_API (STD_ON)
/** \brief Enable/disable Eth get TX stats count API */
#define ETH_GET_TX_STATS_API (STD_ON)
/** \brief Enable/disable Eth get TX error stats count API */
#define ETH_GET_TX_ERROR_COUNTERSVALUES_API (STD_ON)
/** \brief Enable/disable Eth zero-copy transmit API */
#define ETH_ZERO_COPY_TX (STD_OFF)
/** \brief Enable/disable Eth queue-based APIs */
#define ETH_USE_Q_APIS (STD_OFF)
/** \brief Enable/disable Eth MII related API */
#define ETH_ENABLE_MII_API (STD_ON)
/** \brief Enable/disable optional API Eth_UpdatePhysAddrFilter */
#define ETH_UPDATE_PHYS_ADDR_FILTER_API (STD_ON)
/** \brief Enable/disable optional API Eth_NotifyVirtmacMsgReceived */
#define ETH_VIRTUALMAC_NOTIFYMSGRECEIVED_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacSubscribeAllTraffic */
#define ETH_VIRTUALMAC_SUBSCRIBEALLTRAFFIC_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacUnsubscribeAllTraffic */
#define ETH_VIRTUALMAC_UNSUBSCRIBEALLTRAFFIC_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacSubscribeDstMac */
#define ETH_VIRTUALMAC_SUBSCRIBEDSTMAC_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacUnsubscribeDstMac */
#define ETH_VIRTUALMAC_UNSUBSCRIBEDSTMAC_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacAssociateIPv4Macaddr */
#define ETH_VIRTUALMAC_ASSOCIATEIPV4MACADDR_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacDisassociateIPv4Macaddr */
#define ETH_VIRTUALMAC_DISASSOCIATEIPV4MACADDR_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacAddUnicastAddr */
#define ETH_VIRTUALMAC_ADD_UNICAST_MACADDR_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacAddMcastAddr */
#define ETH_VIRTUALMAC_ADD_MCAST_MACADDR_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacDelAddr */
#define ETH_VIRTUALMAC_DEL_MACADDR_API (STD_OFF)
/** \brief Enable/disable optional API Eth_SendCustomNotify */
#define ETH_VIRTUALMAC_SEND_CUSTOM_NOTIFY_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacAddVlan */
#define ETH_VIRTUALMAC_ADD_VLAN_API (STD_OFF)
/** \brief Enable/disable optional API Eth_DispatchVirtmacDelVlan */
#define ETH_VIRTUALMAC_DEL_VLAN_API (STD_OFF)
/** \brief Enable/disable transmit interrupt */
#define ETH_ENABLE_TX_INTERRUPT (STD_ON)
/** \brief Enable/disable receive interrupt */
#define ETH_ENABLE_RX_INTERRUPT (STD_ON)
/** \brief Number of TX buffers */
#define ETH_NUM_TX_BUFFERS (48U)
/** \brief Number of RX buffers */
#define ETH_NUM_RX_BUFFERS (48U)
/** \brief Limits the maximum transmit buffer length (frame length) in bytes */
#define ETH_TX_BUF_LEN_BYTE (1522U)
/** \brief Limits the maximum receive buffer length (frame length) in bytes */
#define ETH_RX_BUF_LEN_BYTE (1522U)
/** \brief Enable/Disable DMA descriptors in cached memory */
#define ETH_DESC_IN_CACHED_MEMORY (STD_ON)
/** \brief Enable/Disable DMA rings in cached memory */
#define ETH_RING_IN_CACHED_MEMORY (STD_ON)
/** \brief ISR type */
#define ETH_ISR_TYPE (ETH_ISR_CAT2)
/** \name Pre-compile switches for MAC addr configuration, ALE conf. etc. */
#define ETH_USE_DEFAULT_MAC_ADDR (STD_OFF)
/** \brief Counter ID for counter used to count wait ticks */
#define ETH_OS_COUNTER_ID ((CounterType)OsCounter_Core0)
/** \brief Timeout value for a wait (busy wait) */
#define ETH_TIMEOUT_DURATION (3200U)
/** \brief MAC address of the controller in network byte order */
#define ETH_CTRL_PHY_ADDRESS { 0xaaU,0xbbU,0xccU,0xddU,0xeeU,0x07U,}
/** \brief Enable/disable Virtual MAC support for CPSW9G */
#define ETH_VIRTUALMAC_SUPPORT (STD_OFF)
/** \brief Timeout value for Firmware Attach msg received from server
* Units of timeout is in terms of number of invocations of Eth_MainFunction
*/
#define ETH_VIRTUALMAC_FWINFO_TIMEOUT (10U)
/* ========================================================================== */
/* External Function Prototype */
/* ========================================================================== */
/** \brief Function to write-back and invalidate cache */
extern void EthApp_wbInvCache(uint8 *buf, uint16 len);
/** \brief Function to write-back cache */
extern void EthApp_wbCache(uint8 *buf, uint16 len);
/** \brief Function to invalidate cache */
extern void EthApp_invCache(uint8 *buf, uint16 len);
/**
* \name ETH DEM Error codes to report
*
* Pre-compile switches for enabling/disabling DEM events
* @{
*/
#define DemConf_DemEventParameter_ETH_DEM_NO_EVENT (0xFFFFU)
#define ETH_DEM_NO_EVENT DemConf_DemEventParameter_ETH_DEM_NO_EVENT
#ifndef ETH_E_HARDWARE_ERROR
/** \brief Hardware failed */
#define ETH_E_HARDWARE_ERROR (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_LATECOLLISION
/** \brief Late collision */
#define ETH_E_LATECOLLISION (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_MULTIPLECOLLISION
/** \brief Multiple collision */
#define ETH_E_MULTIPLECOLLISION (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_SINGLECOLLISION
/** \brief Single collision */
#define ETH_E_SINGLECOLLISION (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_ALIGNMENT
/** \brief Alignment error */
#define ETH_E_ALIGNMENT (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_OVERSIZEFRAME
/** \brief Oversize Frame */
#define ETH_E_OVERSIZEFRAME (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_UNDERSIZEFRAME
/** \brief Undersize frame */
#define ETH_E_UNDERSIZEFRAME (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_CRC
/** \brief CRC Error */
#define ETH_E_CRC (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_RX_FRAMES_LOST
/** \brief Received Frames lost */
#define ETH_E_RX_FRAMES_LOST (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_ACCESS
/** \brief Hardware failed */
#define ETH_E_ACCESS (ETH_DEM_NO_EVENT)
#endif
#ifndef ETH_E_TX_INTERNAL
/** \brief TX packet descriptor returned by UDMA is corrupted.
* Invalid data pointer in descriptor
*/
#define ETH_E_TX_INTERNAL (ETH_DEM_NO_EVENT)
#endif
/* @} */
/* ========================================================================== */
/* Structures and Enums */
/* ========================================================================== */
/* ========================================================================== */
/* Generate Configuration */
/* ========================================================================== */
/**< \brief Pointer to the generated configuration */
extern const struct Eth_ConfigType_s EthConfig_MCU_PC;
/**< \brief Configuration of the driver */
#define ETH_DRV_CONFIG_0 ((const Eth_ConfigType *) &EthConfig_MCU_PC)
/* ========================================================================== */
/* Function Declarations */
/* ========================================================================== */
/* None */
#ifdef __cplusplus
}
#endif
/**< \brief Ethernet configurations
Generated, not expected be modified manually */
ETH_CONFIG_DATA_SECTION CONST(Eth_ConfigType, ETH_CONFIG_DATA)
EthConfig_MCU_PC =
{
.ctrlIdx = ETH_CONTROLLER_ID_0,
/**< Controller index, 0 always */
.udmaInstId = UDMA_INST_ID_MCU_0,
/**< Instance of UDMA to be used */
.dmaTxChIntrNum = 80U,
/**< DMA TX channel interrupt number */
.dmaRxChIntrNum = 81U,
/**< DMA RX channel interrupt number */
.mdioBusFreq = 2200000U,
/**< MDIO bus clock (MDCLK) frequency (in Hz) */
.connType = ETH_MAC_CONN_TYPE_RMII_100,
/**< MII connection type */
.loopback = false,
/**< Loopback enable */
.enableCacheOps = (uint32)TRUE,
/**< Packet memory is cacheable */
.cacheWbInv = (Eth_CacheWbInv) &EthApp_wbInvCache,
/**< Cache write-back invalidate function */
.cacheWb = (Eth_CacheWb) &EthApp_wbCache,
/**< Cache write-back function */
.cacheInv = (Eth_CacheInv) &EthApp_invCache,
/**< Cache invalidate function */
.enetType = ETH_ENETTYPE_CPSW2G,
/**< CPSW type */
.macPort = ETH_PORT_MAC_PORT_1,
/**< Port mode */
.enableVirtualMac = FALSE,
/**< Virtual MAC mode */
};
#define ETH_STOP_SEC_CONFIG_DATA
#include "Eth_MemMap.h"
Below is the sent code during test, which needs to be mounted in the periodic task.
Eth_Init(NULL_PTR);
Eth_SetControllerMode(0, ETH_MODE_ACTIVE);
BufReq_ReturnType Global_TempUSage;
Eth_BufIdxType TmpBuffIdx;
Std_ReturnType EthDemoRetVal;
uint8 ArpData_VLAN3[32] =
{
0x00,0x03,0x08,06,0x00, 0x01, 0x08, 0x00, 0x06, 0x04, 0x00, 0x01, 0x00, 0x03, 0x19, 0x00, 0x00, 0x01,
0xa9, 0xfe, 0xfe, 0xab, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xa9, 0xfe, 0xab, 0xa8
};
uint8 MacDestBrodaddress[6] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};
uint8 MacDestUncastAddress[8] = {0xaa, 0xbb, 0xcc, 0xdd, 0xee, 0x06};
uint8 *TmpBuffPtr;
void Tx_EthFrame_VLAN3(void)
{
boolean Txstatus=0;
uint16 Tmp_Txlenghth1 = 32;
Global_TempUSage[1] = Eth_ProvideTxBuffer(0, 0, &TmpBuffIdx, &TmpBuffPtr, &Tmp_Txlenghth1);
if(TmpBuffPtr != NULL_PTR)
{
TxBufferFill(TmpBuffPtr, Tmp_Txlenghth1, ArpData_VLAN3);
EthDemoRetVal[1] = Eth_Transmit(0, TmpBuffIdx, ETH_VLAN_PROTOCOL, Txstatus, Tmp_Txlenghth1, &MacDestUncastAddress[0]);
}
}
STACK_SIZE = 0x00004000;
Mode_SYS_Stack_Size = 8192;
Mode_EXE_Stack_Size = 1024;
Mode_SVC_Stack_Size = 1024;
Mode_IRQ_Stack_Size = 1024;
Mode_FIQ_Stack_Size = 1024;
OSEE_HEAP_SIZE = 8096;
EXTERN(Memlay_PorstRam_pst)
EXTERN(Memlay_ShareRam_pst)
ENTRY(_start)
MEMORY
{
ATCM (RWX) : ORIGIN = 0x00000000, LENGTH = 0x00007FFF
BTCM (RWX) : ORIGIN = 0x41010000, LENGTH = 0x00007FFF
SRAM (RWX) : ORIGIN = 0x41C02000, LENGTH = 0x41CBFFFF + 1 - 0x41C02000
DDR (RWX) : ORIGIN = 0x80100000, LENGTH = 2M
DDR_DS (RW) : ORIGIN = 0x80300000, LENGTH = 1M
/* DDR for MCU2_1 for Linux resource table [ size 1024 B ] */
DDR_IPC_RESOURCE_TABLE(RW) : ORIGIN = 0xA3300000, LENGTH = 0x400
/* Memory for IPC Vring's. MUST be non-cached or cache-coherent [ size 8.00 MB ] */
DDR_IPC_VRING_MEM(RW) : ORIGIN = 0xA4000000, LENGTH = 8M
/* Dummy area for unspecified input sections. Size 0 */
/* causes an linker error if there is an input section not considered in linker command file. */
must_be_empty : ORIGIN = 0, LENGTH = 0
}
SECTIONS
{
/DISCARD/ : {
*(.comment)
*(.ARM.exidx*)
*(.gnu.linkonce.armexidix.*.*)
}
.vectors : {
. = ALIGN(64);
osee_vector_start = .;
KEEP(*(.vectors))
. = ALIGN(0x80);
osee_vector_end = . - 1;
osee_vector_log2ceil_size = ((osee_vector_end - osee_vector_start) <= (1 << 5) ? 5 : (osee_vector_end - osee_vector_start) <= (1 << 6) ? 6 : (osee_vector_end - osee_vector_start) <= (1 << 7) ? 7 : (osee_vector_end - osee_vector_start) <= (1 << 8) ? 8 :(osee_vector_end - osee_vector_start) <= (1 << 9) ? 9 : (osee_vector_end - osee_vector_start) <= (1 << 10) ? 10 : (osee_vector_end - osee_vector_start) <= (1 << 11) ? 11 : (osee_vector_end - osee_vector_start) <= (1 << 12) ? 12 : (osee_vector_end - osee_vector_start) <= (1 << 13) ? 13 : (osee_vector_end - osee_vector_start) <= (1 << 14) ? 14 : (osee_vector_end - osee_vector_start) <= (1 << 15) ? 15 : (osee_vector_end - osee_vector_start) <= (1 << 16) ? 16 : (osee_vector_end - osee_vector_start) <= (1 << 17) ? 17 : (osee_vector_end - osee_vector_start) <= (1 << 18) ? 18 : (osee_vector_end - osee_vector_start) <= (1 << 19) ? 19 : (osee_vector_end - osee_vector_start) <= (1 << 20) ? 20 : (osee_vector_end - osee_vector_start) <= (1 << 21) ? 21 : (osee_vector_end - osee_vector_start) <= (1 << 22) ? 22 : (osee_vector_end - osee_vector_start) <= (1 << 23) ? 23 : (osee_vector_end - osee_vector_start) <= (1 << 24) ? 24 : (osee_vector_end - osee_vector_start) <= (1 << 25) ? 25 : (osee_vector_end - osee_vector_start) <= (1 << 26) ? 26 : (osee_vector_end - osee_vector_start) <= (1 << 27) ? 27 : (osee_vector_end - osee_vector_start) <= (1 << 28) ? 28 : (osee_vector_end - osee_vector_start) <= (1 << 29) ? 29 : (osee_vector_end - osee_vector_start) <= (1 << 30) ? 30 : (osee_vector_end - osee_vector_start) <= (1 << 31) ? 31 : -1);
} > ATCM
.kernel_bss_percpu (NOLOAD) : ALIGN(8) {
*(osee_kernel_bss_percpu)
} > BTCM
.kernel_data_percpu : ALIGN(8) {
*(osee_kernel_data_percpu)
} > BTCM AT > SRAM
.startup : {
. = ALIGN(64);
*(.startup)
*(osee_boot_kernel_text)
*(.startupCode)
. = ALIGN(8);
} > SRAM
.rodata.ipc : {
*(.rodata.CddIpcConfiguraions_PC)
. = ALIGN(8);
} > SRAM
.bss.ipc_vring_mem (NOLOAD) :
{
*(.bss.ipc_vring_mem)
. = ALIGN(8);
} > DDR_IPC_VRING_MEM
.resource_table :
{
__RESOURCE_TABLE = .;
*(.resource_table)
. = ALIGN(8);
__RESOURCE_TABLE_END = . - 1;
} > DDR_IPC_RESOURCE_TABLE
kernel_code_start_align : {
. = ALIGN(osee_kernel_code_size_to_align);
osee_kernel_code_start = .;
} > DDR
.kernel_text : {
*(.boot)
*(.kernel_text)
*(osee_kernel_text)
*(.gnu.linkonce.t.*)
*(.plt)
*(.gnu_warning)
*(.gcc_execpt_table)
*(.glue_7)
*(.glue_7t)
*(.vfp11_veneer)
*(.ARM.extab)
*(.gnu.linkonce.armextab.*)
} > DDR
OsApplication_Core0_code_start_align : {
osee_OsApplication_Core0_code_start = .;
} > DDR
.OsApplication_Core0_text : ALIGN(8) {
*(osee_OsApplication_Core0_text)
*(*_OsApplication_Core0_text)
} > DDR
OsApplication_Core0_code_stop_align : {
osee_OsApplication_Core0_code_end = .;
} > DDR
.text_cpu0 : {
*(osee_core0_text)
*(*_core0_text.*)
} > DDR
.init : {
KEEP (*(.init))
} > DDR
.fini : {
KEEP (*(.fini))
} > DDR
.interp : {
KEEP (*(.interp))
} > DDR
.note-ABI-tag : {
KEEP (*(.note-ABI-tag))
} > DDR
.ctors : {
__CTOR_LIST__ = .;
___CTORS_LIST___ = .;
KEEP (*crtbegin.o(.ctors))
KEEP (*(EXCLUDE_FILE(*crtend.o) .ctors))
KEEP (*(SORT(.ctors.*)))
KEEP (*(.ctors))
__CTOR_END__ = .;
___CTORS_END___ = .;
} > DDR
.dtors : {
__DTOR_LIST__ = .;
___DTORS_LIST___ = .;
KEEP (*crtbegin.o(.dtors))
KEEP (*(EXCLUDE_FILE(*crtend.o) .dtors))
KEEP (*(SORT(.dtors.*)))
KEEP (*(.dtors))
__DTOR_END__ = .;
___DTORS_END___ = .;
} > DDR
.fixup : {
*(.fixup)
} > DDR
.eh_frame : {
*(.eh_frame)
} > DDR
.eh_framehdr : {
*(.eh_framehdr)
} > DDR
.gcc_except_table : {
*(.gcc_except_table)
} > DDR
kernel_code_stop_align : {
osee_kernel_code_stop = .;
osee_kernel_code_log2ceil_size = ((osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 5) ? 5 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 6) ? 6 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 7) ? 7 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 8) ? 8 :(osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 9) ? 9 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 10) ? 10 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 11) ? 11 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 12) ? 12 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 13) ? 13 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 14) ? 14 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 15) ? 15 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 16) ? 16 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 17) ? 17 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 18) ? 18 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 19) ? 19 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 20) ? 20 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 21) ? 21 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 22) ? 22 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 23) ? 23 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 24) ? 24 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 25) ? 25 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 26) ? 26 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 27) ? 27 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 28) ? 28 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 29) ? 29 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 30) ? 30 : (osee_kernel_code_stop - osee_kernel_code_start) <= (1 << 31) ? 31 : -1);
osee_kernel_code_size_to_align = 1 << osee_kernel_code_log2ceil_size;
. = ALIGN(osee_kernel_code_size_to_align);
osee_kernel_code_end = .;
} > DDR
api_code_start_align : {
. = ALIGN(osee_api_code_size_to_align);
osee_api_code_start = .;
} > DDR
.api_text : {
*(osee_api_text)
*(*_api_text)
} > DDR
.text : {
*(.text)
*(.text.*)
*(*_TEXT_SECTION)
} > DDR
api_code_stop_align : {
osee_api_code_stop = .;
osee_api_code_log2ceil_size = ((osee_api_code_stop - osee_api_code_start) <= (1 << 5) ? 5 : (osee_api_code_stop - osee_api_code_start) <= (1 << 6) ? 6 : (osee_api_code_stop - osee_api_code_start) <= (1 << 7) ? 7 : (osee_api_code_stop - osee_api_code_start) <= (1 << 8) ? 8 :(osee_api_code_stop - osee_api_code_start) <= (1 << 9) ? 9 : (osee_api_code_stop - osee_api_code_start) <= (1 << 10) ? 10 : (osee_api_code_stop - osee_api_code_start) <= (1 << 11) ? 11 : (osee_api_code_stop - osee_api_code_start) <= (1 << 12) ? 12 : (osee_api_code_stop - osee_api_code_start) <= (1 << 13) ? 13 : (osee_api_code_stop - osee_api_code_start) <= (1 << 14) ? 14 : (osee_api_code_stop - osee_api_code_start) <= (1 << 15) ? 15 : (osee_api_code_stop - osee_api_code_start) <= (1 << 16) ? 16 : (osee_api_code_stop - osee_api_code_start) <= (1 << 17) ? 17 : (osee_api_code_stop - osee_api_code_start) <= (1 << 18) ? 18 : (osee_api_code_stop - osee_api_code_start) <= (1 << 19) ? 19 : (osee_api_code_stop - osee_api_code_start) <= (1 << 20) ? 20 : (osee_api_code_stop - osee_api_code_start) <= (1 << 21) ? 21 : (osee_api_code_stop - osee_api_code_start) <= (1 << 22) ? 22 : (osee_api_code_stop - osee_api_code_start) <= (1 << 23) ? 23 : (osee_api_code_stop - osee_api_code_start) <= (1 << 24) ? 24 : (osee_api_code_stop - osee_api_code_start) <= (1 << 25) ? 25 : (osee_api_code_stop - osee_api_code_start) <= (1 << 26) ? 26 : (osee_api_code_stop - osee_api_code_start) <= (1 << 27) ? 27 : (osee_api_code_stop - osee_api_code_start) <= (1 << 28) ? 28 : (osee_api_code_stop - osee_api_code_start) <= (1 << 29) ? 29 : (osee_api_code_stop - osee_api_code_start) <= (1 << 30) ? 30 : (osee_api_code_stop - osee_api_code_start) <= (1 << 31) ? 31 : -1);
osee_api_code_size_to_align = 1 << osee_api_code_log2ceil_size;
. = ALIGN(osee_api_code_size_to_align);
osee_api_code_end = .;
} > DDR
all_const_start_align : {
. = ALIGN(osee_all_const_size_to_align);
osee_all_const_start = .;
} > DDR
.rodata : ALIGN(4) {
*(*_const)
*(*api_const_64)
*(*api_const_32)
*(*api_const_ptr)
*(*api_const_16)
*(*api_const_8)
*(*api_const_bool)
*(*api_const_unspecified)
*(*api_const)
*(*_const_64)
*(*_const_32)
*(*_const_ptr)
*(*_const_16)
*(*_const_8)
*(*_const_bool)
*(*_const_unspecified)
*(*_postbuildstruct)
*(*_postbuildconfig)
*(.rodata)
*(.rodata.*)
*(.rodata1)
*(.rodata1.*)
*(.gnu.linkonce.r.*)
*(.const.devgroup.*)
*(.boardcfg_data)
*(*_CONFIG_SECTION)
. = ALIGN(8) ;
PROVIDE(__clear_table = .);
LONG(0 + ADDR(.kernel_bss_global)); LONG(SIZEOF(.kernel_bss_global));
LONG(0 + ADDR(.kernel_bss)); LONG(SIZEOF(.kernel_bss));
LONG(0 + ADDR(.sbss)); LONG(SIZEOF(.sbss));
LONG(0 + ADDR(.sbss2)); LONG(SIZEOF(.sbss2));
LONG(0 + ADDR(.tbss)); LONG(SIZEOF(.tbss));
LONG(0 + ADDR(.api_bss)); LONG(SIZEOF(.api_bss));
LONG(0 + ADDR(.bss)); LONG(SIZEOF(.bss));
LONG(0 + ADDR(.OsApplication_Core0_bss)); LONG(SIZEOF(.OsApplication_Core0_bss));
LONG(0 + ADDR(.kernel_bss_cpu0)); LONG(SIZEOF(.kernel_bss_cpu0));
LONG(0 + ADDR(.api_bss_cpu0)); LONG(SIZEOF(.api_bss_cpu0));
LONG(-1); LONG(-1);
PROVIDE(__copy_table = .) ;
LONG(LOADADDR(.kernel_data_percpu)); LONG(ADDR(.kernel_data_percpu)); LONG(SIZEOF(.kernel_data_percpu));
LONG(-1); LONG(-1); LONG(-1);
. = ALIGN(8);
} > DDR
.stack_sizes : ALIGN(4) {
osEE_unwind_start = .;
KEEP (*(.stack_sizes))
osEE_unwind_end = .;
} > DDR
all_const_stop_align : {
osee_all_const_stop = .;
osee_all_const_log2ceil_size = ((osee_all_const_stop - osee_all_const_start) <= (1 << 5) ? 5 : (osee_all_const_stop - osee_all_const_start) <= (1 << 6) ? 6 : (osee_all_const_stop - osee_all_const_start) <= (1 << 7) ? 7 : (osee_all_const_stop - osee_all_const_start) <= (1 << 8) ? 8 :(osee_all_const_stop - osee_all_const_start) <= (1 << 9) ? 9 : (osee_all_const_stop - osee_all_const_start) <= (1 << 10) ? 10 : (osee_all_const_stop - osee_all_const_start) <= (1 << 11) ? 11 : (osee_all_const_stop - osee_all_const_start) <= (1 << 12) ? 12 : (osee_all_const_stop - osee_all_const_start) <= (1 << 13) ? 13 : (osee_all_const_stop - osee_all_const_start) <= (1 << 14) ? 14 : (osee_all_const_stop - osee_all_const_start) <= (1 << 15) ? 15 : (osee_all_const_stop - osee_all_const_start) <= (1 << 16) ? 16 : (osee_all_const_stop - osee_all_const_start) <= (1 << 17) ? 17 : (osee_all_const_stop - osee_all_const_start) <= (1 << 18) ? 18 : (osee_all_const_stop - osee_all_const_start) <= (1 << 19) ? 19 : (osee_all_const_stop - osee_all_const_start) <= (1 << 20) ? 20 : (osee_all_const_stop - osee_all_const_start) <= (1 << 21) ? 21 : (osee_all_const_stop - osee_all_const_start) <= (1 << 22) ? 22 : (osee_all_const_stop - osee_all_const_start) <= (1 << 23) ? 23 : (osee_all_const_stop - osee_all_const_start) <= (1 << 24) ? 24 : (osee_all_const_stop - osee_all_const_start) <= (1 << 25) ? 25 : (osee_all_const_stop - osee_all_const_start) <= (1 << 26) ? 26 : (osee_all_const_stop - osee_all_const_start) <= (1 << 27) ? 27 : (osee_all_const_stop - osee_all_const_start) <= (1 << 28) ? 28 : (osee_all_const_stop - osee_all_const_start) <= (1 << 29) ? 29 : (osee_all_const_stop - osee_all_const_start) <= (1 << 30) ? 30 : (osee_all_const_stop - osee_all_const_start) <= (1 << 31) ? 31 : -1);
osee_all_const_size_to_align = 1 << osee_all_const_log2ceil_size;
. = ALIGN(osee_all_const_size_to_align);
osee_all_const_end = .;
} > DDR
core0_kernel_ram_start_align : {
. = ALIGN(osee_core0_kernel_ram_size_to_align);
osee_core0_kernel_ram_start = .;
} > DDR
OsApplication_Core0_ram_start_align : {
osee_OsApplication_Core0_ram_start = .;
} > DDR
.OsApplication_Core0_bss : ALIGN(8) {
*(osee_OsApplication_Core0_bss)
*(*_OsApplication_Core0_bss)
*(*_OsApplication_Core0_bss_64)
*(*_OsApplication_Core0_bss_32)
*(*_OsApplication_Core0_bss_ptr)
*(*_OsApplication_Core0_bss_16)
*(*_OsApplication_Core0_bss_8)
*(*_OsApplication_Core0_bss_bool)
*(*_OsApplication_Core0_bss_unspecified)
*(*_OsApplication_Core0_postbuildbufbss)
. = ALIGN(8);
*(.bss.gEthRxBufMem)
*(.bss.gEthTxBufMem)
*(.bss.gEthCpswTxPkt)
*(.bss.gEthCpswRxPkt)
*(.bss.Cdd_IpcCommChBuf_0)
. = ALIGN(8);
*(.bss.Cdd_IpcCommChBuf_1)
. = ALIGN(8);
*(.bss.Cdd_IpcCommChBuf_2)
. = ALIGN(8);
*(ipc_data_buffer)
. = ALIGN(8);
*(.bss.Cdd_IpcRpMsgCtrlBuffer)
. = ALIGN(8);
*(.bss.*Ipc*)
. = ALIGN(8);
*(.bss.ddr)
} > DDR
.OsApplication_Core0_data : ALIGN(4) {
osee_OsApplication_Core0_data_start = .;
*(osee_OsApplication_Core0_data)
*(*_OsApplication_Core0_data)
*(*_OsApplication_Core0_data_64)
*(*_OsApplication_Core0_data_32)
*(*_OsApplication_Core0_data_ptr)
*(*_OsApplication_Core0_data_16)
*(*_OsApplication_Core0_data_8)
*(*_OsApplication_Core0_data_bool)
*(*_OsApplication_Core0_data_unspecified)
*(*_OsApplication_Core0_postbuildbuf)
*(*_OsApplication_Core0_postbuildbufdata)
} > DDR
. = ALIGN(64);
OsApplication_Core0_ram_stop_align : {
osee_OsApplication_Core0_ram_end = .;
} > DDR
.kernel_bss_cpu0 : ALIGN(8) {
*(osee_core0_bss)
*(*_core0_bss)
. = ALIGN(8);
} > DDR
.kernel_data_cpu0 : ALIGN(4) {
*(osee_core0_data)
*(*_core0_data)
} > DDR
core0_kernel_ram_stop_align : {
osee_core0_kernel_ram_stop = .;
osee_core0_kernel_ram_log2ceil_size = ((osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 5) ? 5 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 6) ? 6 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 7) ? 7 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 8) ? 8 :(osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 9) ? 9 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 10) ? 10 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 11) ? 11 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 12) ? 12 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 13) ? 13 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 14) ? 14 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 15) ? 15 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 16) ? 16 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 17) ? 17 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 18) ? 18 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 19) ? 19 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 20) ? 20 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 21) ? 21 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 22) ? 22 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 23) ? 23 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 24) ? 24 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 25) ? 25 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 26) ? 26 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 27) ? 27 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 28) ? 28 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 29) ? 29 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 30) ? 30 : (osee_core0_kernel_ram_stop - osee_core0_kernel_ram_start) <= (1 << 31) ? 31 : -1);
osee_core0_kernel_ram_size_to_align = 1 << osee_core0_kernel_ram_log2ceil_size;
. = ALIGN(osee_core0_kernel_ram_size_to_align);
osee_core0_kernel_ram_end = .;
} > DDR
kernel_ram_start_align : {
. = ALIGN(osee_kernel_ram_size_to_align);
osee_kernel_ram_start = .;
} > SRAM
.kernel_bss (NOLOAD) : ALIGN(8) {
osEE_bss_start = .;
*(.bss_cpu)
*(ioc_kernel_bss)
*(osee_kernel_bss)
*(osee_core*_kernel_bss)
*(*_kernel_bss)
*(.gnu.linkonce.b.*)
*(COMMON)
. = ALIGN(8);
osEE_bss_end = .;
} > SRAM
.kernel_bss_global (NOLOAD) : ALIGN(8) {
*(osee_gbl_kernel_bss)
} > SRAM
.tbss : ALIGN(8) {
*(.tbss)
*(.tbss.*)
*(.gnu.linkonce.tb.*)
. = ALIGN(8);
} > SRAM
.sbss (NOLOAD) : ALIGN(8) {
osEE_sbss_start = .;
*(.sbss)
*(.sbss.*)
*(.gnu.linkonce.sb.*)
. = ALIGN(8);
osEE_sbss_end = .;
} > SRAM
.sbss2 : ALIGN(8) {
*(.sbss2)
*(.sbss2.*)
*(.gnu.linkonce.sb2.*)
. = ALIGN(8);
} > SRAM
.kernel_data : ALIGN(4) {
osee_kernel_data_start = .;
*(.data_cpu*)
*(ioc_kernel_data)
*(osee_kernel_data)
*(osee_core*_kernel_data)
*(*_kernel_data)
*(.gnu.linkonce.d.*)
} > SRAM
.kernel_data_global : ALIGN(8) {
*(osee_gbl_kernel_data)
} > SRAM
.data1 : ALIGN(4) {
*(.data1)
*(.data1.*)
} > SRAM
.sdata : ALIGN(4) {
*(.sdata)
*(.sdata.*)
*(.gnu.linkonce.s.*)
} > SRAM
.sdata2 : ALIGN(4) {
*(.sdata2)
*(.sdata2.*)
*(.gnu.linkonce.s2.*)
} > SRAM
.tdata : ALIGN(4) {
*(.tdata)
*(.tdata.*)
*(.gnu.linkonce.td.*)
} > SRAM
.heap (NOLOAD) : ALIGN(64) {
end = .;
} > SRAM
kernel_ram_stop_align : {
osee_kernel_ram_stop = .;
osee_kernel_ram_log2ceil_size = ((osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 5) ? 5 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 6) ? 6 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 7) ? 7 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 8) ? 8 :(osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 9) ? 9 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 10) ? 10 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 11) ? 11 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 12) ? 12 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 13) ? 13 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 14) ? 14 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 15) ? 15 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 16) ? 16 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 17) ? 17 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 18) ? 18 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 19) ? 19 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 20) ? 20 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 21) ? 21 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 22) ? 22 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 23) ? 23 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 24) ? 24 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 25) ? 25 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 26) ? 26 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 27) ? 27 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 28) ? 28 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 29) ? 29 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 30) ? 30 : (osee_kernel_ram_stop - osee_kernel_ram_start) <= (1 << 31) ? 31 : -1);
osee_kernel_ram_size_to_align = 1 << osee_kernel_ram_log2ceil_size;
. = ALIGN(osee_kernel_ram_size_to_align);
osee_kernel_ram_end = .;
} > SRAM
api_ram_start_align : {
. = ALIGN(osee_api_ram_size_to_align);
osee_api_ram_start = .;
} > SRAM
.api_bss (NOLOAD) : ALIGN(8) {
*(osee_api_bss)
*(*_api_bss_32)
*(*_api_bss_ptr)
*(*_api_bss_16)
*(*_api_bss_8)
*(*_api_bss_bool)
*(*_api_bss_unspecified)
*(*_api_bss)
*(*_api_postbuildbufbss)
. = ALIGN(8);
} > SRAM
.bss (NOLOAD) : ALIGN(8) {
*(.bss)
*(.bss.*)
} > SRAM
.api_data : ALIGN(4) {
osee_api_data_start = .;
*(osee_api_data)
*(*_api_data_ptr)
*(*_api_data_32)
*(*_api_data_16)
*(*_api_data_8)
*(*_api_data_bool)
*(*_api_data_unspecified)
*(*_api_data)
*(*_api_postbuildbuf)
*(*_api_postbuildbufdata)
} > SRAM
.data : ALIGN(8) {
*(.data)
*(.data.*)
*(*_DATA_INIT_*_SECTION)
} > SRAM
api_ram_stop_align : {
osee_api_ram_stop = .;
osee_api_ram_log2ceil_size = ((osee_api_ram_stop - osee_api_ram_start) <= (1 << 5) ? 5 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 6) ? 6 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 7) ? 7 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 8) ? 8 :(osee_api_ram_stop - osee_api_ram_start) <= (1 << 9) ? 9 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 10) ? 10 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 11) ? 11 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 12) ? 12 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 13) ? 13 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 14) ? 14 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 15) ? 15 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 16) ? 16 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 17) ? 17 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 18) ? 18 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 19) ? 19 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 20) ? 20 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 21) ? 21 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 22) ? 22 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 23) ? 23 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 24) ? 24 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 25) ? 25 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 26) ? 26 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 27) ? 27 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 28) ? 28 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 29) ? 29 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 30) ? 30 : (osee_api_ram_stop - osee_api_ram_start) <= (1 << 31) ? 31 : -1);
osee_api_ram_size_to_align = 1 << osee_api_ram_log2ceil_size;
. = ALIGN(osee_api_ram_size_to_align);
osee_api_ram_end = .;
} > SRAM
core0_api_ram_start_align : {
. = ALIGN(osee_core0_api_ram_size_to_align);
osee_core0_api_ram_start = .;
} > SRAM
.api_bss_cpu0 : ALIGN(8) {
*(osee_core0_api_bss)
*(*_core0_api_bss)
. = ALIGN(8);
} > SRAM
.api_data_cpu0 : ALIGN(4) {
*(osee_core0_api_data)
*(*_core0_api_data)
} > SRAM
core0_api_ram_stop_align : {
osee_core0_api_ram_stop = .;
osee_core0_api_ram_log2ceil_size = ((osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 5) ? 5 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 6) ? 6 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 7) ? 7 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 8) ? 8 :(osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 9) ? 9 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 10) ? 10 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 11) ? 11 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 12) ? 12 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 13) ? 13 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 14) ? 14 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 15) ? 15 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 16) ? 16 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 17) ? 17 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 18) ? 18 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 19) ? 19 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 20) ? 20 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 21) ? 21 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 22) ? 22 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 23) ? 23 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 24) ? 24 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 25) ? 25 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 26) ? 26 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 27) ? 27 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 28) ? 28 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 29) ? 29 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 30) ? 30 : (osee_core0_api_ram_stop - osee_core0_api_ram_start) <= (1 << 31) ? 31 : -1);
osee_core0_api_ram_size_to_align = 1 << osee_core0_api_ram_log2ceil_size;
. = ALIGN(osee_core0_api_ram_size_to_align);
osee_core0_api_ram_end = .;
} > SRAM
os_stack_start_align : {
. = ALIGN(osee_os_stack_size_to_align);
osee_os_stack_start = .;
} > SRAM
.stack (NOLOAD) : ALIGN(64) {
*(.stack)
} > SRAM
. += 32;
. = ALIGN(32);
osee_OsApplication_Core0_stack_start = .;
. = ALIGN(1024);
.OsApplication_Core0_stack : ALIGN(4) {
*(osee_OsApplication_Core0_stack)
*(*_OsApplication_Core0_stack)
} > SRAM
. = ALIGN(32);
osee_OsApplication_Core0_stack_end = .;
. += 32;
. = ALIGN(32);
.cpu0.stack (NOLOAD): ALIGN(16) {
osee_core0_stack_start = .;
*(.stack_cpu0)
*(.ustack_cpu0*)
. = ALIGN(8);
PROVIDE(osee_core0_sys_stack_top = .);
. += Mode_SYS_Stack_Size;
. = ALIGN(8);
PROVIDE(osee_core0_sys_stack = .);
PROVIDE(osee_core0_sys_stack_bottom = .);
osEE_core0_svc_stack_top = .;
. += Mode_SVC_Stack_Size;
osEE_core0_svc_stack_bottom = .;
. = ALIGN(8);
PROVIDE(osee_core0_svc_stack = .);
osEE_core0_irq_stack_top = .;
. += Mode_IRQ_Stack_Size;
osEE_core0_irq_stack_bottom = .;
. = ALIGN(8);
PROVIDE(osee_core0_irq_stack = .);
osEE_core0_fiq_stack_top = .;
. += Mode_FIQ_Stack_Size;
osEE_core0_fiq_stack_bottom = .;
. = ALIGN(8);
PROVIDE(osee_core0_fiq_stack = .);
osEE_core0_abt_stack_top = .;
. += Mode_EXE_Stack_Size;
osEE_core0_abt_stack_bottom = .;
. = ALIGN(8);
PROVIDE(osee_core0_abt_stack = .);
osEE_core0_und_stack_top = .;
. += Mode_EXE_Stack_Size;
osEE_core0_und_stack_bottom = .;
. = ALIGN(8);
PROVIDE(osee_core0_und_stack = .);
osee_core0_stack_end = .;
} > SRAM
os_stack_stop_align : {
osee_os_stack_stop = .;
osee_os_stack_log2ceil_size = ((osee_os_stack_stop - osee_os_stack_start) <= (1 << 5) ? 5 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 6) ? 6 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 7) ? 7 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 8) ? 8 :(osee_os_stack_stop - osee_os_stack_start) <= (1 << 9) ? 9 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 10) ? 10 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 11) ? 11 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 12) ? 12 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 13) ? 13 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 14) ? 14 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 15) ? 15 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 16) ? 16 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 17) ? 17 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 18) ? 18 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 19) ? 19 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 20) ? 20 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 21) ? 21 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 22) ? 22 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 23) ? 23 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 24) ? 24 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 25) ? 25 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 26) ? 26 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 27) ? 27 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 28) ? 28 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 29) ? 29 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 30) ? 30 : (osee_os_stack_stop - osee_os_stack_start) <= (1 << 31) ? 31 : -1);
osee_os_stack_size_to_align = 1 << osee_os_stack_log2ceil_size;
. = ALIGN(osee_os_stack_size_to_align);
osee_os_stack_end = .;
} > SRAM
.caldata :
{
__DS_CALDATA_START = .;
*(.caldata.asw)
. = ALIGN(8);
__DS_CALDATA_LVL2_START = .;
*(.caldata.lvl2)
. = ALIGN(8);
__DS_CALDATA_LVL2_END = . - 1;
*(.caldata)
. = ALIGN(8);
__DS_CALDATA_END = . - 1;
} > DDR_DS
/***********************************************************/
/* virtual sections without memory */
/***********************************************************/
.debug_aranges 0 : { *(.debug_aranges) }
.debug_macinfo 0 : { *(.debug_macinfo) }
.debug_abbrev 0 : { *(.debug_abbrev) }
.debug_info 0 : { *(.debug_info) }
.debug_line 0 : { *(.debug_line) }
.debug_frame 0 : { *(.debug_frame) }
.debug_ranges 0 : { *(.debug_ranges) }
.debug_str 0 : { *(.debug_str) }
.debug_loc 0 : { *(.debug_loc) }
.ARM.attributes 0 : { *(.ARM.attributes)}
.rel.plt 0 : { *(.rel.plt) }
.rel.dyn 0 : { *(.rel.dyn) }
.symtab 0 : { *(.symtab) }
.symtab_shndxr 0 : { *(.symtab_shndxr) }
.shstrtab 0 : { *(.shstrtab) }
.strtab 0 : { *(.strtab) }
.unspecified_sections : { *(*) } > must_be_empty
}
Could you help check this case? Thanks.
Best Regards,
Cherry