Other Parts Discussed in Thread: OMAP-L138, OMAPL138, OMAP-L137
Hello, I am using a custom board with OMAP-L138 And SPI flash of ATMEL AT45DB321D. I flashed the SPI using CCS4 with spi-flash-writer( I had to add support for ATMEL since the spi-flash-writer 3.20.00.XX does not include support for atmel). Anyway, I get that the application succeed in reading with the text "File Match". I flashed first arm-spi-ais.bin - "armais" file, but after reseting in mode booting from SPI1 flash (0x0C in boot configuration register), I get no printing at all in UART. I tried to change page size from 528 to 512, and flashed again the armais file but still nothing... Can it be that OMAP cannot boot from ATMEL, or is there anything else wrong in my configuration ? I thank you for your help, Ran Shalit