Platform:EVM 6472
version: 3.20.04.68
IPC: 1.21.02.23
BIOS: 6.30.03.46
XDAIS: 6.25.01.08
Platform:EVM 6472
version: 3.20.04.68
IPC: 1.21.02.23
BIOS: 6.30.03.46
XDAIS: 6.25.01.08
CCS4.0
My CCS4.0 often close unexpected when I load the program on the six cores and run it simultaneously. But when I just
load the program on one core of six , the unexpected situation only occurs several times. The following is the
configuration of eclipse in eclipse.ini . My computer has 4 cores and 2G memory.
Who can tell me how to configure CCS so that it can works well?
eclipse.ini:
-vmargs
-Xms40m
-Xmx1024m
-XX:MaxPermSize=96m