Hi,
When I user emmc boot it will stuck at " A start job is running for udev Wai…ice Initialization" about 3 minutes ?
What shoud I do ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When I user emmc boot it will stuck at " A start job is running for udev Wai…ice Initialization" about 3 minutes ?
What shoud I do ?
Hi,
I believe you are able to boot to Linux command prompt but you are seeing a 3 minute delay with a user space task during boot. Can you confirm the same and also share the complete boot logs for us to analyse?
Also which SDK version are you using?
Regards,
Keerthy
Hi Keerthy,
Our sdk linux version is 5.10.100
And I find that I add "systemctl mask systemd-udev-settle" will pass it after next boot.