Part Number: AM625
Other Parts Discussed in Thread: TPS65219
Where to change CPU frequency? seems it is no in .dts. how about to support configuration in .dts?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tony,
Dynamic Frequency Scaling will be supported. But I don't see "opp-microvolt" property is defined in the device tree OPP table, so I don't think Dynamic Voltage Scaling is supported.
Bin,
If AM62x support Dynamic Frequency Scaling, it is hard to understand not support Dynamic Voltage Scaling, From SOC perspective, if dynamic change frequency need SW and DM firmware involved, may cause some potential problem, but for Dynamic Voltage Scaling, SOC even doesn't know external voltage changed as long as power supply can maintain SOC activity. if frequency decreased. lower voltage can meet SOC activity.
Hi Tony,
SDK v8.4 is currently planed to be released by end of September.
At this moment, customers can change CPU frequency to 1.4HGz using k3conf command, just please ensure the VDD_CORE is at 0.85v.
# k3conf set clock 135 0 1400000000