Hi,
We are using custom SDK 8.1 and we are using it on custom TDA4 Board.
Setting continuous MAC address from the Linux side causes the following errors:
[MCU2_0] 4326.034814 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a3848194,CoreKey:38acb7e6, MacAddress:2:0:0:10:5:4, FlowIdx:172, FlowIdxOffset:0
[MCU2_0] 4326.035218 s: CpswAle_ioctl: Failed to set policer: -8
[MCU2_0] 4326.035277 s: Cpsw_ioctlInternal: Failed to set DSTMAC policer: -8
[MCU2_0] 4326.078460 s: EnetAppUtils_regDstMacRxFlow() failed CPSW_ALE_IOCTL_SET_POLICER: -8
Any pointers on this error.
Following are the script that we keep trying continuously
ifconfig eth0 down
ifconfig eth0 hw ether $mac
ifconfig eth0 up