Other Parts Discussed in Thread: TEST2
Hello Champs,
Customer failed to run the AM625 rtos demo in C:\ti\mcu_plus_sdk_am62x_08_03_00_07\examples\drivers\mcan\mcan_loopback_interrupt. He only added some printf code.
Below are the tests he did.
1. build and run the polling mode code, this internal loopback code send 8 bytes then receive, the TX 32bit ID and data are the same to RX 32bit ID and data. The test is successful.
2. build and run the interrupt mode code, this code is can FD internal loopback mode. send 64bytes and then receive, the TX 32bit ID and data are not the same to RX 32bit ID and data. 32bit ID FD variable rate are all 0. There is only higher 8 bytes in data. The test failed. Please see below is the log.
3. Modify the above test1 polling code to can fd mode, the phenomena is the same to test2.
4. The can fd example in linux is correct.

Thanks.
Rgds
Shine