This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: MCAN actual transfer rate

Part Number: AM625

Could you tell me the actual transfer rate for MCAN?

The TRM describes that the bit rate can be programmed to values greater than 1 Mbps.

TI products include CAN transceivers that support 2 Mbps, 5 Mbps, and 8 Mbps.

Can the MCAN support 2Mbps, 5Mbps or 8Mbps?

Best regards,

Daisuke