Other Parts Discussed in Thread: DM3730
Hello,
In my design, there are some switches between the LPDDR memory chip and DM3730. The trace length ends up to be 3.5 ~ 4 inches and lumped capacitance ~11pF. Will this be OK with programming Drive Strength to proper level (Full, three-quarter, half)? I can add series termination resistor to make impedance match. My concern is: the output impedance of the devices (memory and DM) is not constant. It changes with output voltage as well as process and temperature. So perfect impedance match is not possible. There will be some overshoot and undershoot.
By the way, the memory chip to be used is MT46H128M16LFCK (60-ball).
Thanks a lot!
--Bill