This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: About Errata SPRZ303H Advisory2.3.18

Part Number: TMS320C6748

Our board has a TMS320C6748 on it. The 1.8V I/F is not used. And the 1.8V power supply  is generated from the 3.3V power supply using an LDO and supplied to the C6748. Therefore, as shown in this errata, 1.8V rises to nearly 3V. However, the C6748 seems to work just fine. Will anything go wrong with the C6748 if I allow 1.8V to go up to 3V?