Hello,
If I want to interface a 16 bit RGB (QVGA) LCD to AM3715 DSS, which Pins are used as dss_data[15:0] or dss_data[23:8] ?
And also, what is the exact sequence to configure the RGB 16-bit LCD output ?
Thanks,
Ali.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If I want to interface a 16 bit RGB (QVGA) LCD to AM3715 DSS, which Pins are used as dss_data[15:0] or dss_data[23:8] ?
And also, what is the exact sequence to configure the RGB 16-bit LCD output ?
Thanks,
Ali.
Ali,
Have a look at the following Wiki for some information which may help you...
http://processors.wiki.ti.com/index.php/Display_Subsystem
BR,
Steve