This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Am facing the following error while i click on Export DCC binary. I am getting this error on all the plugins, regardless of the input. Not sure what could have gone wrong. Need help on this.
The screenshots i have attached above is all, after clicking the process button.
2. I have been using this tool for sometime now! I did generate xml's 2 days back also. It is weird how it doesn't work all of a sudden, with similar errors on all the pc.
Just a Guess, is there time limit on these tools by chance or some kind of cache issue!!?
This is weird!
There is no time limit for the tool.
If you reboot your PC and/or start a new project from scratch, do you still have the same issue?
Ah ! I just tried it twice. No luck on that either.
Open DCC>plugins>load image>set params>click"process button"
Is there anything more I should do? i am losing my reailty here ! Ha Ha. Really Weird.
Could you please try opening the test project below?
Go to H3A plugin and then click the process button.
I see below message after the clicking before going to the export button.
Could you please try "menu/Execute/Reset current plugin" and then click process button?
Thanks for trying and hopefully this can fix your issues.
Not sure what is going wrong on your side.
Typically, starting a new project from scratch should work if anything is broken in your current project/plugin.
Resetting current plugin should have the same effect.