This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: Cold Software Reset does not assert nRESETIN_OUT

Part Number: AM3358


Hi,

Our customer is doing an evaluation on a board made overseas.
They are writing 0x02 to PRM_RSTCTRL Register and doing SW cold reset. The reset is applied, but the nRESETIN_OUT is not asserted.
Looking at Reset out Assertion (nRESETIN_OUT Pin) in Table 8-26. of the TRM, there seems to be no specific condition. What could be the reason why it is not asserted?
The pull-up on nRESETIN_OUT is 10 ohms and nRESETIN_OUT does not seem to be asserted when they change the value of the PRM_RSTTIME Register.

Best Regards,

Kouji Nishigata