HI All,
we are using codecs which we downloaded from TI site (dvsdk_3_10_00_16 version) along with GIT kernel 2.6.32 on DM6467T.
when we are try to decode .264 file of resolution 1920x1080i. and the file been little corrupt using TI's decode application provided
with the dvsdk ,we observe artifacts on OSD.
Actually the artifacts/gliches in output occur when it tries to decode the corrupt part of the file, but the decoder output doesn't recover(shows glitches) even if
the file is good later .
When we play the same file on media player like VLC it plays seamlessly.
could you please let us know what could be the problem, i have attached the input file for verification.
please change the extension to .264
H.264 decoder version is 01.10.04.
Regards,
Bhushan.