Part Number: TDA4VM
Hello Team,
We are not able to get the Ethernet link status (eth0) in Linux(A72).
SDK version is :
RTOS : ti-processor-sdk-rtos-j721e-evm-08_01_00_13
Linux : ti-processor-sdk-linux-j7-evm-08_01_00_07-Linux
If ethernet is disconnected and ifconfig is triggered then also status is UP as mentioned in below log.
root@j7-evm:/# ifconfig
eth0 Link encap:Ethernet HWaddr 02:00:00:10:05:00
inet addr:192.168.x.x Bcast:192.168.7.255 Mask:255.255.255.0
inet6 addr: fe80::ff:fe10:500/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:3696 errors:0 dropped:0 overruns:0 frame:0
TX packets:3831 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:363471 (354.9 KiB) TX bytes:3352320 (3.1 MiB)
root@j7-evm:/# cat /sys/class/net/eth0/operstate
unknown