This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: How to interpret a Crash Output: Resource conflict exception

Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAPL138, SYSBIOS

Hello Team, and thank you for the support. 

Are you able to please help me understand this "Resource conflict exception" ?  It does not happen very often, when hooking up to the debugger. 

Our code is standard code from the pdk_omapl138_1_0_11 SDK.  We have USB, I2C and UART, using the I2C and UART transaction examples.  We are using the USB host example.  

Any ideas please ?   Is it something we should be concerned about ?

[C674X_0] A0=0x0 A1=0x1
A2=0x4 A3=0x0
A4=0x0 A5=0x0
A6=0x0 A7=0x0
A8=0xc0911660 A9=0x0
A10=0xc0921104 A11=0x14000103
A12=0xc08e4768 A13=0xc0016ba0
A14=0x20 A15=0xffffffff
A16=0xc0923e34 A17=0x40
A18=0x0 A19=0x0
A20=0x4000 A21=0xc0924940
A22=0x92de063b A23=0x4000
A24=0xc0946fb0 A25=0x0
A26=0x14 A27=0xc0945e3c
A28=0x1 A29=0x3
A30=0xe A31=0x0
B0=0xc0948dc4 B1=0xc0946698
B2=0xc0948dc4 B3=0x14
B4=0xf8 B5=0xc0946860
B6=0xc0948dc4 B7=0x0
B8=0xc0908a88 B9=0x0
B10=0x0 B11=0xc0948da0
B12=0xc091a8c8 B13=0xc0946698
B14=0xc0945e58 B15=0xc0946698
B16=0x0 B17=0xc0946db0
B18=0xc0922fb4 B19=0xc0946db0
B20=0xc08c676c B21=0xc0946698
B22=0x1be30200 B23=0xc0946698
B24=0xc08c6768 B25=0x14
B26=0x1bb40300 B27=0xc0946698
B28=0xc08c7a04 B29=0xc08c7a20
B30=0x0 B31=0xc0946698
NTSR=0xc000a2f8
ITSR=0x1c8e0200
IRP=0xc08cf7f0
SSR=0xc0946698
AMR=0x1c8e0200
RILC=0xc0946698
ILC=0xc08cf7e0
Exception at 0xc08fc718
EFR=0x2 NRP=0xc08fc718
Internal exception: IERR=0x10
Resource conflict exception
ti.sysbios.family.c64p.Exception: line 265: E_exceptionMax: pc = 0xc0946698, sp = 0xc0946698.
xdc.runtime.Error.raise: terminating execution