This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

regarding leopard dm355 ridge run

hi

we are trying to make the kernel

by make cmd but the error given below is coming

our dir is work/leo365 where we have downloaded the rr from repository link

and all the essential packages we have installed

dm365@dm365-desktop:~/work/leo365$ make

Ridgerun Linux SDK
  Board configuration: Leopard Board DM365
 
  Processing toolchain...
    Build complete
  Processing kernel...
    Applying quilt patches to the kernel linux-2.6.32...
  
Usage: quilt [--trace[=verbose]] [--quiltrc=XX] command [-h] ...
       quilt --version
Commands are:

Global options:

--trace
    Runs the command in bash trace mode (-x). For internal debugging.

--quiltrc file
    Use the specified configuration file instead of ~/.quiltrc (or
    /etc/quilt.quiltrc if ~/.quiltrc does not exist).  See the pdf
    documentation for details about its possible contents.

--version
    Print the version number and exit immediately.
make[1]: *** [patches] Error 255
make: *** [kernel_build] Error 2

 

 

can anyone shortout the prob

thanx

kailash