Other Parts Discussed in Thread: AB15, AM625
Hi ,
could you please share the info about LVDS and how to configure in DTS and as well as in kernel .
Thanks,
Naresh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
could you please share the info about LVDS and how to configure in DTS and as well as in kernel .
Thanks,
Naresh
Hi Krunal ,
Thanks for patch dual display patch.
actually our setup is single channel display ,accordingly we configured the LVDS in device tree .
we just observed light vertical lines on the display .
please let us know what are the changes required to make get the LVDS display
we got the kmstest and modetest response as below :
oot@am62xx-evm:/sys/class/drm/card0-LVDS-1# kmsprint
[ 2965.061449] line=88 fun=panel_lvds_get_modes
Connector 0 (39) LVDS-1 (connected)
Encoder 0 (38) LVDS
Crtc 0 (37) 1280x800 68.200 1280/64/1/5 800/40/1/2 60 (59.93)
Plane 0 (31) fb-id: 47 (crtcs: 0) 0,0 1280x800 -> 0,0 1280x800 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YU)
FB 47 1280x800
Plane 1 (40) fb-id: 51 (crtcs: 0) 0,0 1280x800 -> 0,0 1280x800 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YU)
FB 51 1280x800
root@am62xx-evm:/sys/class/drm/card0-LVDS-1# kmstest
[ 2969.758164] line=88 fun=panel_lvds_get_modes
Could not get DRM master permission. Card already in use?
root@am62xx-evm:/sys/class/drm/card0-LVDS-1# modetest -M tidss
[ 3564.430778] line=88 fun=panel_lvds_get_modes
Encoders:
id crtc type possible crtcs possible clones
38 37 LVDS 0x00000001 0x00000001
Connectors:
id encoder status name size (mm) modes encoders
39 38 connected LVDS-1 153x117 1 38
modes:
index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
#0 1280x800 59.93 1280 1344 1345 1350 800 840 841 843 68200 flags: ; type: preferred, driver
props:
1 EDID:
flags: immutable blob
blobs:
value:
2 DPMS:
flags: enum
enums: On=0 Standby=1 Suspend=2 Off=3
value: 0
5 link-status:
flags: enum
enums: Good=0 Bad=1
value: 0
6 non-desktop:
flags: immutable range
values: 0 1
value: 0
4 TILE:
flags: immutable blob
blobs:
value:
20 CRTC_ID:
flags: object
value: 37
CRTCs:
id fb pos size
37 47 (0,0) (1280x800)
#0 1280x800 59.93 1280 1344 1345 1350 800 840 841 843 68200 flags: ; type: preferred, driver
props:
22 ACTIVE:
flags: range
values: 0 1
value: 1
23 MODE_ID:
flags: blob
blobs:
value:
680a0100000540054105460500002003
480349034b0300003c00000000000000
48000000313238307838303000000000
00000000000000000000000000000000
00000000
19 OUT_FENCE_PTR:
flags: range
values: 0 18446744073709551615
value: 0
24 VRR_ENABLED:
flags: range
values: 0 1
value: 0
27 CTM:
flags: blob
blobs:
value:
28 GAMMA_LUT:
flags: blob
blobs:
value:
29 GAMMA_LUT_SIZE:
flags: immutable range
values: 0 4294967295
value: 256
Planes:
id crtc fb CRTC x,y x,y gamma size possible crtcs
31 37 47 0,0 0,0 0 0x00000001
formats: AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12
props:
8 type:
flags: immutable enum
enums: Overlay=0 Primary=1 Cursor=2
value: 1
17 FB_ID:
flags: object
value: 47
18 IN_FENCE_FD:
flags: signed range
values: -1 2147483647
value: -1
20 CRTC_ID:
flags: object
value: 37
13 CRTC_X:
flags: signed range
values: -2147483648 2147483647
value: 0
14 CRTC_Y:
flags: signed range
values: -2147483648 2147483647
value: 0
15 CRTC_W:
flags: range
values: 0 2147483647
value: 1280
16 CRTC_H:
flags: range
values: 0 2147483647
value: 800
9 SRC_X:
flags: range
values: 0 4294967295
value: 0
10 SRC_Y:
flags: range
values: 0 4294967295
value: 0
11 SRC_W:
flags: range
values: 0 4294967295
value: 83886080
12 SRC_H:
flags: range
values: 0 4294967295
value: 52428800
32 zpos:
flags: range
values: 0 1
value: 0
33 COLOR_ENCODING:
flags: enum
enums: ITU-R BT.601 YCbCr=0 ITU-R BT.709 YCbCr=1
value: 0
34 COLOR_RANGE:
flags: enum
enums: YCbCr limited range=0 YCbCr full range=1
value: 0
35 alpha:
flags: range
values: 0 65535
value: 65535
36 pixel blend mode:
flags: enum
enums: Pre-multiplied=0 Coverage=1
value: 0
40 37 51 0,0 0,0 0 0x00000001
formats: AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12
props:
8 type:
flags: immutable enum
enums: Overlay=0 Primary=1 Cursor=2
value: 0
17 FB_ID:
flags: object
value: 51
18 IN_FENCE_FD:
flags: signed range
values: -1 2147483647
value: -1
20 CRTC_ID:
flags: object
value: 37
13 CRTC_X:
flags: signed range
values: -2147483648 2147483647
value: 0
14 CRTC_Y:
flags: signed range
values: -2147483648 2147483647
value: 0
15 CRTC_W:
flags: range
values: 0 2147483647
value: 1280
16 CRTC_H:
flags: range
values: 0 2147483647
value: 800
9 SRC_X:
flags: range
values: 0 4294967295
value: 0
10 SRC_Y:
flags: range
values: 0 4294967295
value: 0
11 SRC_W:
flags: range
values: 0 4294967295
value: 83886080
12 SRC_H:
flags: range
values: 0 4294967295
value: 52428800
41 zpos:
flags: range
values: 0 1
value: 1
42 COLOR_ENCODING:
flags: enum
enums: ITU-R BT.601 YCbCr=0 ITU-R BT.709 YCbCr=1
value: 0
43 COLOR_RANGE:
flags: enum
enums: YCbCr limited range=0 YCbCr full range=1
value: 0
44 alpha:
flags: range
values: 0 65535
value: 65535
45 pixel blend mode:
flags: enum
enums: Pre-multiplied=0 Coverage=1
value: 0
Frame buffers:
id size pitch
root@am62xx-evm:/sys/class/drm/card0-LVDS-1#
thanks ,
Naresh
hi Krunal
We are trying to bring up LVDS on AM625- custom platform,
The patch is for Dual channel LVDS , but we are using single channel (using port@0 only) for our LVDS setup
The output of kmstest as below , (display shows some lines)
root@am62xx-evm:~# killall -9 weston ; kmsprint ; kmstest -c LVDS-1 -r 1280x800
killall: weston: no process killedton ; kmsprint ; kmstest -c LVDS-1 -r 1280x800
Connector 0 (39) LVDS-1 (connected)
Encoder 0 (38) LVDS
Crtc 0 (37) 1280x800 68.200 1280/64/2/5 800/40/1/2 60 (59.88)
Plane 0 (31) fb-id: 46 (crtcs: 0) 0,0 1280x800 -> 0,0 1280x800 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12)
FB 46 1280x800
Connector 0/@39: LVDS-1
Crtc 0/@37: 1280x800 68.200 1280/64/2/5/? 800/40/1/2/? 60 (59.88) 0 0x48
Plane 0/@31: 0,0-1280x800
Fb 47 1280x800-XR24
press enter to exit
below is LCD output :
-nagendra

Okay, have you gone through the patches to understand how we enabled dual link? Here is an example of what a customer did to use our patches and enable single link panel: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1128751/am625-oldi-driver-or-dts-example/4199484#4199484
Regards,
Krunal
Hi Krunal ,
we followed the same which one of the customer did for single channel display in that thread , even though our disaplay not getting .[ which appears as we posted in prevoius thread ].
may i know what's these settings for ->
uenvcmd=if run check_psdk_setup; then echo "Already setup."; else run do_psdk_setup; mw.b ${loadaddr} 0 1; fatwrite mmc 1:1 ${loadaddr} .psdk_setup 1; reset; fi; mw.l 0x00109008 0x68EF3490; mw.l 0x0010900C 0xD172BC5A; mw.l 0x00108700 0x00000000;
Thanks,
Naresh
The Uboot change enables the OLDITX IP because by default they are powered off. Please share the LCD dts file.
Regards,
Krunal
Hi Naresh,
The DTS file looks okay and have you tried to probe the PCLK/data lines to ensure everything is meeting your spec? Also, please check with your LCD vendor to ensure timing parameters are correct.
Regards,
Krunal
Hi Krunal
we could get the LVDS clock-0 and data lines toggling , the clock is matching with our configured value (signals, OLDI0_A0/A2/A3/A4 and OLDI0_CLK0)
-nagendra
Hello nagendra,
My recommendation would be to check with the timing parameters of your LCD. On my setup, I got a single channel LVDS to work and here are my changes:
diff --git a/arch/arm64/boot/dts/ti/k3-am625-sk-oldi-panel.dts b/arch/arm64/boot/dts/ti/k3-am625-sk-oldi-panel.dts
index 600955e89a06..d8d87c654eac 100644
--- a/arch/arm64/boot/dts/ti/k3-am625-sk-oldi-panel.dts
+++ b/arch/arm64/boot/dts/ti/k3-am625-sk-oldi-panel.dts
@@ -25,31 +25,24 @@
data-mapping = "vesa-24";
panel-timing {
- clock-frequency = <150280000>;
- hactive = <1920>;
- vactive = <1200>;
- hback-porch = <32>;
- hfront-porch = <52>;
- vback-porch = <24>;
- vfront-porch = <8>;
- hsync-len = <24>;
- vsync-len = <3>;
+ clock-frequency = <71100000>;
+ hactive = <1280>;
+ vactive = <800>;
+ hback-porch = <48>;
+ hfront-porch = <32>;
+ vback-porch = <2>;
+ vfront-porch = <5>;
+ hsync-len = <80>;
+ vsync-len = <16>;
de-active = <1>;
};
port@0 {
- dual-lvds-even-pixels;
lcd_in0: endpoint {
remote-endpoint = <&oldi_out0>;
};
};
- port@1 {
- dual-lvds-odd-pixels;
- lcd_in1: endpoint {
- remote-endpoint = <&oldi_out1>;
- };
- };
};
};
};
@@ -66,18 +59,8 @@
AM62X_IOPAD(0x026c, PIN_OUTPUT, 0) /* (AA8) OLDI0_A2P */
AM62X_IOPAD(0x0278, PIN_OUTPUT, 0) /* (AB6) OLDI0_A3N */
AM62X_IOPAD(0x0274, PIN_OUTPUT, 0) /* (AA7) OLDI0_A3P */
- AM62X_IOPAD(0x0280, PIN_OUTPUT, 0) /* (AC6) OLDI0_A4N */
- AM62X_IOPAD(0x027c, PIN_OUTPUT, 0) /* (AC5) OLDI0_A4P */
- AM62X_IOPAD(0x0288, PIN_OUTPUT, 0) /* (AE5) OLDI0_A5N */
- AM62X_IOPAD(0x0284, PIN_OUTPUT, 0) /* (AD6) OLDI0_A5P */
- AM62X_IOPAD(0x0290, PIN_OUTPUT, 0) /* (AE6) OLDI0_A6N */
- AM62X_IOPAD(0x028c, PIN_OUTPUT, 0) /* (AD7) OLDI0_A6P */
- AM62X_IOPAD(0x0298, PIN_OUTPUT, 0) /* (AD8) OLDI0_A7N */
- AM62X_IOPAD(0x0294, PIN_OUTPUT, 0) /* (AE7) OLDI0_A7P */
AM62X_IOPAD(0x02a0, PIN_OUTPUT, 0) /* (AD4) OLDI0_CLK0N */
AM62X_IOPAD(0x029c, PIN_OUTPUT, 0) /* (AE3) OLDI0_CLK0P */
- AM62X_IOPAD(0x02a8, PIN_OUTPUT, 0) /* (AE4) OLDI0_CLK1N */
- AM62X_IOPAD(0x02a4, PIN_OUTPUT, 0) /* (AD5) OLDI0_CLK1P */
>;
};
};
@@ -98,24 +81,4 @@
remote-endpoint = <&lcd_in0>;
};
};
-
- /* VP1: LVDS Output (OLDI TX 1) */
- port@2 {
- reg = <2>;
- oldi_out1: endpoint {
- remote-endpoint = <&lcd_in1>;
- };
- };
-};
-
-&main_i2c1 {
- #address-cells = <1>;
- #size-cells = <0>;
-
- touchscreen@41 {
- compatible = "ilitek,ili251x";
- reg = <0x41>;
- interrupt-parent = <&exp1>;
- interrupts = <15 IRQ_TYPE_EDGE_FALLING>;
- };
};
The timing varies based on the manufacture so verify your datasheet.
Regards,
Krunal
hello Krunal
yes we verified our timings are correct, all LVDS signals are toggling as expected (A0-A3) , clk0 is observed as expected
still, we could not get our display working, the output on lvds display is as before
since drm/card0-lvds node is present and all signals are toggling , can we rule out software dependency ?
-Nagendra
Yes, I don't think it's a software dependency. Also, if you run kmstest, does your LVDS node enumerate? Also, it should print the timing values that corresponds to the DTS entry. If the answer is yes, we know the driver is configured and DSS IP is sending the correct signals to the panel.
Regards,
Krunal
Krunal
yes, the kmstest provides the timing details according to our DTB , also LVDS node info , and activity observed in all LVDS signals
any suggestion to check and confirm HW side ?

-nagendra
Are you observing the gradient issue on all the panels or just one? Also, you may have to probe clock and pixel data simultaneously and ensure all the data is latching on the appropriate falling edge or rising edge. Also, check with the panel vendor on possible issues that could contribute to gradients. Also, please ensure that data-mapping "vesa-24" matches your panel requirement.
Regards,
Krunal