Other Parts Discussed in Thread: SYSBIOS
MessageQ and Notify are used at the same time
I want to use MessageQ and Notify in the same project. First, I just added "var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ'); var HeapBufMP = xdc.useModule'ti.sdo.ipc.heaps.HeapBufMP')" to nofity_single.cfg and didn't edit the notify_single.c. But when the program run in six cores, IPC is not syncing without any console. Who can tell me how to add the MessageQ to the notify project and let them works at the same project? Should I comment the sentence "var Notify = xdc.useModule('ti.sdo.ipc.Notify');" when I use the MessageQ code? Can Notify and MessageQ be used in a project? Notify_single.cfg is as follws.
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.setConfig(null, ["CORE0", "CORE1", "CORE2",
"CORE3", "CORE4", "CORE5"]);
var System = xdc.useModule('xdc.runtime.System');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
/* Modules explicitly used in the application */
var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ');
var HeapBufMP = xdc.useModule('ti.sdo.ipc.heaps.HeapBufMP');
var Notify = xdc.useModule('ti.sdo.ipc.Notify');
var Ipc = xdc.useModule('ti.sdo.ipc.Ipc');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Memory = xdc.useModule('xdc.runtime.Memory');
Memory.defaultHeapSize = 0x40000;
Program.heap = 0x40000;
Program.sectMap["emacComm"] = "DDR2";
Program.sectMap[".text"] = "DDR2";
Program.sectMap[".far"] = "DDR2";
/* Synchronize all processors (this will be done in Ipc_start) */
Ipc.procSync = Ipc.ProcSync_ALL;
/* Shared Memory base address and length */
var SHAREDMEM = 0x200000;
var SHAREDMEMSIZE = 0xA0000;
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
SharedRegion.setEntryMeta(0,
{ base: SHAREDMEM,
len: SHAREDMEMSIZE,
ownerProcId: 0,
isValid: true,
name: "SL2_RAM",
});
var Global = xdc.useModule('ti.ndk.config.Global');
Global.enableCodeGeneration = false;
/* Create a semaphore with count 0 */
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
Program.global.semHandle = Semaphore.create(0);
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
Program.global.sem = Semaphore.create(0);
var instSemaphore0Params0 = new Semaphore.Params();
instSemaphore0Params0.instance.name = "sem";
Program.global.sem = Semaphore.create(0, instSemaphore0Params0);
Platform:EVM 6472
XDCtools version: 3.20.04.68
IPC: 1.21.02.23
BIOS: 6.30.03.46
XDAIS: 6.25.01.08