Part Number: TDA4VM
Hi,
So, I was trying to install the TDA4 SDK on Ubuntu 20.04. It showed an error message that Ubuntu 20.04 is not supported and the process would abort. After digging it, I found that by simply adding the Ubuntu 20.04 version option in the installation script, the install was successful. Additionally, it also showed that gcc-5 was required which is not part of the recent Ubuntu versions, and I needed to install gcc-5 manually for the SDK to be installed successfully. I have these questions,
1. Why is the install not supported on Ubuntu 20.04?
2. What is consequence of making the install happen like the way I mentioned above? Will there be any issues with creating the artifacts and porting them to the board, on Ubuntu 20.04?
3. Why is gcc-5/g++-5 required? Could it be made possible to work with gcc-9?
Finally, if the above-mentioned issues are not critical for development, please remove these errors/dependency in the next releases.