This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAM-3517 Mounting Rootfile system from NFS fails

Other Parts Discussed in Thread: AM3517, ADS7846

Texas Instruments X-Loader 1.47 (Mar 24 2011 - 15:54:47) Booting from nand . . .ment variables Starting OS Bootloader... showvar - print local hu U-Boot 2010.06-rc1 (Mar 24 2011 - 15:55:56) sleep - delay execution for OMAP34xx/35xx-GP ES1.0, CPU-OPP2 L3-165MHz source - run script from memory TAM3517 TWISTER Board + LPDDR/NAND - minimal test like /bin/sh I2C: ready DRAM: 256 MiBboot image via NAND: 256 MiBTFTP protocol In: serial Out: serial tr Err: serialhing, success Customer/Vender : TechNexion version - print m Project/Board : tam3517 TAM35 Sequence Number : 1052000000000069and - NAND sub-system revision : TN15 1.0 mmc1 is avail eth0 addr : 00:1F:7B:15:01:10 eth1 addr : 00:1F:7B:15:01:11 eth2 addr : 0 TAM3517 # boot TAM3517 # TAM3517 # TAM3517 # setenv serverip 192.168.1.233 TAM3517 # setenv netmask 255.255.255.0 TAM3517 # setenv bootfile 'uImage' TAM3517 # boot TAM3517 # setenv bootargs console=ttyS0,115200n8 noinitrd mem=256M root=/dev/nfs rw nfsroot=192.168.1.233:/var/lib/tftpboot,noloc TAM3517 # setenv bootcmd 'dhcp 80008000 uImage; bootm' TAM3517 # saveenv Saving Environment to NAND... Erasing Nand... Erasing at 0x180000 -- 100% complete. Writing to Nand... done TAM3517 # boot BOOTP broadcast 1 DHCP client bound to address 192.168.1.18 Using DaVinci EMAC device TFTP from server 192.168.1.233; our IP address is 192.168.1.18 Filename 'uImage'. Load address: 0x80008000 Loading: ##########T #########################T #########################T ##### ####################T ################## ################################################################# ##########################T #########################T ############## ############T ############T ######################################T ### ##################################T ############################### #######T ########################################################## ##############################T #########################T ###### done Bytes transferred = 2639884 (28480c hex) ## Booting kernel from Legacy Image at 80008000 ... Image Name: Linux-2.6.32 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2639820 Bytes = 2.5 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK Starting kernel ... Uncompressing Linux............................................................. ................................................................................ ........................ done, booting the ker Linux version 2.6.32 (root@localhost.localdomain) (gcc version 4.5.1 (Sourcery G ++ Lite 2010.09-50) ) #1 Thu May 26 18:40:59 IST 2011 CPU: ARMv7 Processor [411fc087] revision 7 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: TAM3517 EVM Memory policy: ECC disabled, Data cache writeback AM3517 ES1.0 (l2cache iva sgx neon isp ) SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x100000 Reserving 10485760 bytes SDRAM for VRAM Built 1 zonelists in Zone order, mobil Kernel command line: console=ttyS0,115200n8 noinitrd mem=256M root=/dev/nfsrw nf sroot=192.168.1.233:/var/lib/tftpboot,nolock,ip=dhcp init=/init PID hash table entries: 1024 (order: 0, 4096 bytes) Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Memory: 256MB = 256MB total Memory: 243712KB available (4624K code, 821K data, 160K init, 0K highmem) Hierarchical RCU implementation. NR_IRQS:368 Clocking rate (Crystal/Core/MPU): 26.0/332/500 GPMC revision 5.0 IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts Total of 96 interrupts on 1 active controller OMAP GPIO hardware version 2.5 OMAP clockevent source: GPTIMER1 at 32768 Hz Console: colour dummy device 80x30 Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696) Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok regulator: core version 0.5 NET: Registered protocol family 16 mux: Could not set signal i2c2_scl mux: Could not set signal i2c2_sda mux: Could not set signal i2c3_scl mux: Could not set signal i2c3_sda Display initialized successfully OMAP DMA hardware revision 4.0 bio: create slab at 0 SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb i2c_omap i2c_omap.1: bus 1 rev3.12 at 400 kHz regulator: VDCDC1: 1200 mV normal regulator: VDCDC2: 3300 mV normal regulator: VDCDC3: 1800 mV normal regulator: LDO1: 1800 mV normal regulator: LDO2: 3300 mV normal i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz Bluetooth: Core ver 2.15 NET: Registered protocol family 31 Bluetooth: HCI device and connection manager initialized Bluetooth: HCI socket layer initialized cfg80211: Calling CRDA to update world regulatory domain Switching to clocksource 32k_counter musb_hdrc: version 6.0, cppi4.1-dma, otg (peripheral+host), debug=0 AM3517 OTG revision 4ea41001, PHY f0036e2, control 00 musb_hdrc: USB OTG mode controller at d0810000 using DMA, IRQ 71 NET: Registered protocol family 2 IP route cache hash table entries: 2048 (order: 1, 8192 bytes) TCP established hash table entries: 8192 (order: 4, 65536 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes) TCP: Hash tables configured (established 8192 bind 8192) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. AM3517 Linux PSP version 03.00.01.06 (TAM3517) NetWinder Floating Point Emulator V0.97 (double precision) ashmem: initialized VFS: Disk quotas dquot_6.5.2 Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) squashfs: version 4.0 (2009/01/31) Phillip Lougher JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc. msgmni has been set to 476 alg: No test for stdrng (krng) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) OMAP DSS rev 2.0 OMAP DISPC rev 3.0 OMAP VENC rev 2 OMAP DSI rev 1.0 Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654 console [ttyS0] enabled serial8250.1: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654 serial8250.2: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654 brd: module loaded loop: module loaded at24 1-0050: 256 byte 24c02 EEPROM (writab at24 2-0050: 256 byte 24c02 EEPROM (writable) SCSI Media Changer driver v0.25 omap2-nand driver initializing NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bi t) Creating 5 MTD partitions on "omap2-nand.0": 0x000000000000-0x000000080000 : "xloader" 0x000000080000-0x000000180000 : "uboot" 0x000000180000-0x0000001a0000 : "params" 0x0000001a0000-0x0000007a0000 : "kernel" 0x0000007a0000-0x000010000000 : "rootfs" vcan: Virtual CAN interface driver CAN device driver interface TI High End CAN Controller Driver 0.7 ti_hecc ti_hecc.1: device registered (reg_base=d08e0000, irq=24) smsc911x: Driver version 2008-10-21. smsc911x-mdio: probed eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1) net eth0: MAC Address: 4e:4d:9a:d3:26:e0 usbcore: registered new interface driver cdc_ether ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver ehci-omap ehci-omap.0: OMAP-EHCI Host Controller ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1 ehci-omap ehci-omap.0: irq 77, io mem 0x48064800 ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: OMAP-EHCI Host Controller usb usb1: Manufacturer: Linux 2.6.32 ehci_hcd usb usb1: SerialNumber: ehci-omap.0 hub 1-0:1.0: USB hub found hub 1-0:1.0: 3 ports detected Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. android init f_acm init android_register_function acm f_adb init android_register_function adb f_mass_storage init android_register_function usb_mass_storage f_rndis init android_register_function rndis mice: PS/2 mouse device common for all mice ads7846 spi1.0: touchscreen, irq 296 input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input 0 using rtc device, ds1307, for alarms rtc-ds1307 3-0068: rtc core: registered ds1307 as rtc0 rtc-ds1307 3-0068: 56 by i2c /dev entries driver Linux video capture interface: v2.00 OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec Bluetooth: Virtual HCI driver ver 1.3 Bluetooth: HCI UART driver ver 2.2 Bluetooth: HCI H4 protocol initialized Bluetooth: HCI BCSP protocol initialized Bluetooth: HCILL protocol initialized Bluetooth: Broadcom Blutonium firmware driver ver 1.2 usbcore: registered new interface driver bcm203x Bluetooth: Digianswer Bluetooth USB driver ver 0.10 usbcore: registered new interface driver bpa10x Bluetooth: BlueFRITZ! USB driver ver 1.2 usbcore: registered new interface driver bfusb Bluetooth: Generic Bluetooth USB driver ver 0.6 usbcore: registered new interface driver btusb Bluetooth: Generic Bluetooth SDIO driver ver 0.1 Registered led device: status omap_pwm_led omap_pwm_led.1: OMAP PWM LED (bklight) at GP timer 9/0 Registered led device: bklight usbcore: registered new interface driver usbhid usbhid: USB HID core driver logger: created 64K log 'log_main' logger: created 256K log 'log_events' logger: created 64K log 'log_radio'May 9 2011 - 16:49:13) logger: created 64K log 'log_system' Booting from nand . . . Advanced Linux Sound Architecture Driver Version 1.0.21. U-Boot 2010.06-rc1 (Jan 28 2011 - 14:26:1 usbcore: registered new interface driver snd-usb-audio/35xx-GP ES1.0, CPU-OPP2 L3-165MHz No device for DAI tlv320aic23 TWISTER Board + LPDDR/NAND No device for DAI omap-mcbsp-dai-0C: ready DRAM: 256 No device for DAI omap-mcbsp-dai-1 In: serial No device for DAI omap-mcbsp-dai-2: serial Customer/V No device for DAI omap-mcbsp-dai-3 Project/Board : tam3 No device for DAI omap-mcbsp-dai-4ce Number : 1052000000000069 TAM3517 EVM SoC init revision AIC23 Audio Codec 0.1 et asoc: tlv320aic23 <-> omap-mcbsp-dai-0 mapping ok eth1 addr : 00:1F:7B:15:01: ALSA device list: #0: tam3517 (tlv0 serverip=192.168.1.4 Bluetooth: L2CAP ver 2.14=ttyS0,115200n8 Bluetooth: L2CAP socket layer initializedth=eth1 mpurate=600 Bluetooth: SCO (Voice Link) ver 0.6 nandparts=omap2-nand.0:512k(xload Bluetooth: SCO socket layer initialized,-(root Bluetooth: RFCOMM TTY layer initialized fs) disp_mode_0=set def_dis Bluetooth: RFCOMM socket layer initializedngs=8000,480/8 Bluetooth: RFCOMM ver 1.11 davinci_emac_probe: using random MAC addr: ee:27:c0:67:6b:ca280x720@60 emac-mii: probed disp_mode_4= rtc-ds1307 3-0068: setting system clock to 2011-05-27 22:59:50 UTC (1306537190) disp_mode_5=set def_disp tv;set disp_mode omapfb Root-NFS: unknown option: ip=dhcp usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0 usb 1-1: Product: USB2.0 Hub hub 1-1:1.0: USB hub found hub 1-1:1.0: 4 ports detected usb 1-1.1: new high speed USB device using ehci-omap and address 3 usb 1-1.1: New USB device found, idVendor=05e3, idProduct=0718 usb 1-1.1: New USB device strings: Mfr=0, Product=1, SerialNumber=2 usb 1-1.1: Product: USB Storage usb 1-1.1: SerialNumber: 000000000033 scsi0 : usb-storage 1-1.1:1.0 scsi 0:0:0:0: Direct-Access USB TO I DE/SATA Device 0015 PQ: 0 ANSI: 0 sd 0:0:0:0: Attached scsi generic sg0 type 0 sd 0:0:0:0: [sda] Attached SCSI disk rpcbind: server 192.168.1.233 not responding, timed out Root-NFS: Unable to get nfsd port number from server, using default Looking up port of RPC 100005/1 on 192.168.1.233 rpcbind: server 192.168.1.233 not responding, timed out Root-NFS: Unable to get mountd port number from server, using default Root-NFS: Server returned error -101 while mounting /var/lib/tftpboot VFS: Unable to mount root fs via NFS, trying floppy. VFS: Cannot open root device "nfsrw" or unknown-block(2,0) Please append a correct "root=" boot option; here are the available partitions: Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

  • Your root=/dev/nfsrw is incorrect. There should be a space between s and r so that

    root=/dev/nfs rw

    Steve K.

  • Dear Sir, In my above post the environment vcariables have been set for the same but the after executing the command it takes it as root=/dev/nfsrw instead of root=/dev/nfs rw and hence i overwritten the command and corrected it and booted but same problem arises and the output goes with same error. I have a dought is it something with the NFS server is not authenticating access please look at this... rpcbind: server 192.168.1.233 not responding, timed out Root-NFS: Unable to get nfsd port number from server, using default Looking up port of RPC 100005/1 on 192.168.1.233 rpcbind: server 192.168.1.233 not responding, timed out Root-NFS: Unable to get mountd port number from server, using default Root-NFS: Server returned error -101 while mounting /var/lib/tftpboot VFS: Unable to mount root fs via NFS, trying floppy. and here it gives error for the incorrect bootargs --> but previous to this is some server errror i think so VFS: Cannot open root device "nfsrw" or unknown-block(2,0) Please append a correct "root=" boot option; here are the available partitions: Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0) Thanks and regards hrishikesh.