Hi,
I want complete the function that cpsw2 can connect cpsw9 by the way of mac to mac. But the cpsw2 is controlled by A72 core not R5 core, then what should I do? My linux sdk version is 08_02_00, rtos sdk version is 08_02_00_06
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want complete the function that cpsw2 can connect cpsw9 by the way of mac to mac. But the cpsw2 is controlled by A72 core not R5 core, then what should I do? My linux sdk version is 08_02_00, rtos sdk version is 08_02_00_06
Hi,
For MAC2MAC connections, you would need a fixed-link node in the ethernet port node of mcu_cpsw. You would need to update the "cpsw_port1" node in "[PSDK-Linux Istall Dir]/board-support/linux-[Commit-hash]/arch/arm64/boot/dts/ti/k3-j721e-common-proc-board.dts" to include the fixed-link node. You also have to remove the "phy-handle" property in "cpsw_port1" node. Reference :
&cpsw_port1 { phy-mode = "rgmii-rxid"; // phy-handle = <&phy0>; fixed-link { speed = <1000>; full-duplex; }; };