This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

video loop-back Setting for PAL 576i



hi all:

I am using tvp-5150 for encoder and  connect to DM365 C[0-7]. Camera is PAL.

test code is from SpectrulDigital, I have changed some appropriately. here is the code:

static void vpfe_init( Uint32 ntsc_pal_mode )

{

    Uint32 width;

    Uint32 height;

    if ( ntsc_pal_mode == NTSC )

    {

        width   = 720;

        height  = 480;

    }

    else

    {

        width   = 720;

        height  = 576; //change to 576

    }


    ISIF_SYNCEN =  0x0000;  // Disable VPFE during setup

    ISIF_MODESET = 0x2F84;  // Interlaced, VD priority as negative

    ISIF_HDW     = 0x0000;

    ISIF_VDW     = 0x0000;

    ISIF_PPLN    = 0x02CF;  // 720

    if(ntsc_pal_mode == NTSC)

    ISIF_LPFR    = 0x020D;  // 526

    else

    ISIF_LPFR = 626;

    /*

     *  sph = 1, nph = 1440, according to the CCDC spec

     *  for BT.656 mode, this setting captures only the 720x480 of the

     *  active NTSV video window

     */

    ISIF_SPH     = 0x0000;

    ISIF_LNH     = width << 1;                 // * Horizontal lines

    ISIF_HSIZE   = width >> 4;                 // Horizontal line offset

    ISIF_SLV0    = 0x0000;                     // Vertical start line

    ISIF_SLV1    = 0x0000;

    ISIF_LNV     = height >> 1;                // Vertical lines

    ISIF_CULH    = 0xffff;                     // Disable culling

    ISIF_CULV    = 0x00ff;

    /*

     *  Interleave the two fields

     */

    ISIF_SDOFST      = 0x0249;                 // Line offset

//dm355 is 0

    ISIF_CADU        = 0x0400;                 // Frame buffer address high,old=0x0400, why is 0x0400?

    ISIF_CADL        = 0x0000;                 // Frame buffer address low

//dm355 is 3

   ISIF_REC656IF    = 0x0001;                 // REC656 enabled,old=1

    /*

     *  Input format is Cb:Y:Cr:Y, w/ Y in odd-pixel position

     */

    //ISIF_CCDCFG      = 0x0812;                 // CCD configuration

    ISIF_CCDCFG      = 0x0802;                 // CCD configuration,0x10 = swap C/Y

    ISIF_FMTCFG      = 0x0000;                 // Disable formatter

    ISIF_FMTSPH      = 0x0000;

    ISIF_FMTLNH      = 0x02D0;

    ISIF_FMTSLV      = 0x0000;

    ISIF_FMTLNV      = 0x0000;

    ISIF_SYNCEN      = 0x0003;                 // Enable CCDC

}

//  back end **********************************************************************

static void vpbe_init( Uint32 colorbar_loopback_mode, Uint32 ntsc_pal_mode, Uint32 output_mode )

{

    Uint32 video_buffer = DDR_BASE + ( DDR_SIZE / 2 );

    Uint32 basep_x;

    Uint32 basep_y;

    Uint32 width;

    Uint32 height;

    if ( ntsc_pal_mode == NTSC )

    {

        basep_x = 0x7A; // 122

        basep_y = 0x12; // 18

        width   = 720;

        height  = 480;

    }

    else

    {

        basep_x = 0x84; // 132

        basep_y = 0x16; // 22

        width   = 720;

        height  = 576; //change to 576

    }

    /*

     * Setup clocking / DACs

     */

    VDAC_CONFIG         = 0x081141CC;   // Take DACs out of power down mode

    VPSS_CLKCTL         = 0x00000018;   // Enable DAC and VENC clock, both at 27 MHz

    VPSS_VPBE_CLK_CTRL  = 0x00000011;   // Select enc_clk*1, turn on VPBE clk

    VENC_CLKCTL         = 0x00000001;   // Enable venc 

    /*

     * Setup OSD

     */

    OSD_MODE       = 0x000000fc;   // Blackground color blue using clut in ROM0

    OSD_OSDWIN0MD  = 0;            // Disable both osd windows and cursor window

    OSD_OSDWIN1MD  = 0;

    OSD_RECTCUR    = 0;

if(colorbar_loopback_mode == COLORBARS)

    {

    OSD_VIDWIN0OFST = width >> 4;

    OSD_VIDWIN0ADR = video_buffer;

}else //loopback

{

OSD_VIDWIN0OFST = 0x1000 | width >> 4; //width >> 4 donot work! why?

OSD_VIDWIN0ADR = video_buffer;

}

    OSD_BASEPX     = basep_x;

    OSD_BASEPY     = basep_y;

    OSD_VIDWIN0XP  = 0;

    OSD_VIDWIN0YP  = 0;

    OSD_VIDWIN0XL  = width;

    OSD_VIDWIN0YL  = height >> 1;

    OSD_MISCCTL    = 0;

    OSD_VIDWINMD   = 0x00000003;   // Disable vwindow 1 and enable vwindow 0

                                        // Frame mode with no up-scaling

    /*

     *  Setup VENC

     */

    if ( ntsc_pal_mode == NTSC )

        VENC_VMOD  = 0x00000003;   // Standard NTSC interlaced output

    else

        VENC_VMOD  = 0x00001243;   // Standard PAL interlaced output,old=0x0043

    VENC_VDPRO     = colorbar_loopback_mode << 8;

    VENC_VDPRO    |= 0x200;  // 100% Color bars

    VENC_DACTST    = 0;

    /*

     *  Choose Output mode

     */

    if ( output_mode == COMPOSITE_OUT )

        VENC_DACSEL = 0x00000000;

    else if ( output_mode == SVIDEO_OUT )

        VENC_DACSEL = 0x00004210;

}

static Int16 video_colorbars_test(void)

{

    /* Setup Back-End */

    vpbe_init( COLORBARS, PAL, COMPOSITE_OUT );

    return 0;

}

static Int16 video_loopback_test(void)

{

    vpfe_init( PAL);

    /* Setup Back-End */

    vpbe_init( LOOPBACK, PAL, COMPOSITE_OUT );

    return 0;

}

But I find no COLOR in some monitor (both ColorBar and Loopback), but some monitor has color.

And when testing loop-back ,I can see some blink like water wave from the video, can I program the register to solve this problem?

Thanks.

  • YJ Liu,

    YJ Liu said:
    But I find no COLOR in some monitor (both ColorBar and Loopback), but some monitor has color.

    Do you mean to say that some video comes up properly OR is it some invalid color? Please post some screenshots, that will help us to understand the problem better.

    YJ Liu said:
    And when testing loop-back ,I can see some blink like water wave from the video, can I program the register to solve this problem?

    snapshots will help in this case too.



  • Hi,Nagabhushana:

    Thanks for replying. The "water wave" cannot be seen from snapshot, sorry for that.

    I have two monitors, one is professional monitor( for CCD Camera Factory Manufacturing test) and the other is a analog LCD panel( accept CVBS).

    From the professional one I cannot see any color , what i mean is the picture become gray. But from the LCD Panel , I can see the color (not gray anymore).

    I prefer to believing the result from the PROFESSIONAL Monitor , So I think the CVBS signal is lacking something :)

    what do you think?

  • hi nagabhushan,

    i am also facing same problem for dm355evm,

    Getting output for both color_bars and video loopback,

    but black and white video .

    Thanks and Regards,

    Mohammed Asif.