This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515, CSL UART compiler error

 

Hi,

I am using CSL UART example and trying to build the project but I got  these 2 errors.

1) cannot find file "Debug/cslVC5505.lib"

2) file "C:/Program Files/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.8/lib/rts55x.lib<exit.obj>" has a Tag_Memory_Model attribute value of "2" that is different than one previously seen ("3"); combining incompatible files 

I have searched on e2e forum and by referring http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/110/t/11147.aspx  I have complied cslVC5505 program from TMS320C55XXCSL-LOWPWR\c55xx_csl\ccs_v4.0_examples  now I have cslVC5505.lib file in My workspace debug folder but my problem is not solved.

Whenever I build my project I get above errors.

Am I missing something?

 

Regards,

Sakshi