Other Parts Discussed in Thread: SYSBIOS
I am trying to use hookset functionality for Hwi, Tasks in sysbios. I could not understand, how to use them. Can anybody have any examples?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSBIOS
I am trying to use hookset functionality for Hwi, Tasks in sysbios. I could not understand, how to use them. Can anybody have any examples?
Hi Rahul,
I've attached a .c and .cfg that shows an example of Task hook functions. Below is the output on a C64+ device.
Todd
myRegister1: assigned HookSet Id = 0
myRegister2: assigned HookSet Id = 1
myCreate1: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0x0
myCreate2: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0x0
myReady1: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0xdead1
myReady2: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0xdead2
myCreate1: task name = 'myTsk0', pEnv = 0x0
myCreate2: task name = 'myTsk0', pEnv = 0x0
myReady1: task name = 'myTsk0', pEnv = 0xdead1
myReady2: task name = 'myTsk0', pEnv = 0xdead2
ti.sysbios.heaps.HeapMem: line 296: out of memory: handle=0x80e1e0, size=2048
xdc.runtime.Error.raise: terminating execution
myRegister1: assigned HookSet Id = 0
myRegister2: assigned HookSet Id = 1
myCreate1: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0x0
myCreate2: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0x0
myReady1: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0xdead1
myReady2: task name = 'ti.sysbios.knl.Task.IdleTask', pEnv = 0xdead2
myCreate1: task name = 'myTsk0', pEnv = 0x0
myCreate2: task name = 'myTsk0', pEnv = 0x0
myReady1: task name = 'myTsk0', pEnv = 0xdead1
myReady2: task name = 'myTsk0', pEnv = 0xdead2
mySwitch1: ignoring dummy 1st prev Task
next name = 'myTsk0', pNextEnv = 0xc0de1
mySwitch2: ignoring dummy 1st prev Task
next name = 'myTsk0', pNextEnv = 0xc0de2
myTsk0 Entering
myTsk0 Calling Task_yield
mySwitch1: prev name = 'myTsk0', pPrevEnv = 0xc001c0de
next name = 'myTsk0', pNextEnv = 0xc0de0ff1
mySwitch2: prev name = 'myTsk0', pPrevEnv = 0xc002c0de
next name = 'myTsk0', pNextEnv = 0xc0de0ff2
myTsk0 Exiting
myExit1: curTask name = 'myTsk0', pEnv = 0xc001c0de
myExit2: curTask name = 'myTsk0', pEnv = 0xc002c0de
mySwitch1: prev name = 'myTsk0', pPrevEnv = 0xdedbeef1
next name = 'ti.sysbios.knl.Task.IdleTask', pNextEnv = 0xc0de1
mySwitch2: prev name = 'myTsk0', pPrevEnv = 0xdedbeef2
next name = 'ti.sysbios.knl.Task.IdleTask', pNextEnv = 0xc0de2
Entering idleFunc().
myDelete1: task name = 'myTsk0', pEnv = 0xc0de0ff1
myDelete2: task name = 'myTsk0', pEnv = 0xc0de0ff2
Hi Todd,
Thank you for your reply. Examples are very helpful. I have the following questions.
1. If there are multiple HookSet functions, Do all HookSet functions will be called corresponding to a task operation? For example, if there are mySwitch1,mySwitch2,mySwitch3 hook functions for a Task switch operation, Do all three mySwitch1,mySwitch2,mySwitch3 functions will be called whenever a Task switch happens?. If yes, what is the advantage of having multiple HookSet functions?
2. In .cfg sysbios file, when I clicked and highlighted the "ti.sysbios.knl.Task", I see a "hooks" field in the properties window. But, when I clicked and highlighted the "ti.sysbios.hal.Hwi", I don't see "hooks" field in the properties window. Does this mean, hook functions are not supported for Hwi or am I missing anything in the setup?
3. I read in the sysbios documentation that the Hook functions are also supported for HWI, SWI. If I have to add the hooks for HWI, Do I have to write in the similar way as Tasks in your example? Below is an example:
Hwi.addHookSet({
registerFxn: '&myRegister1',
createFxn: '&myCreate1',
beginFxn: '&myReady1',
endFxn: '&mySwitch1',
deleteFxn: '&myDelete1',
});
Thanks a lot,
Rahul
Hi Rahul,
#1: Each hook set is called. This allows different developers (or middle-ware) providers to have their own set of hooks. If there was only one set, management would be be harder to coordinate.
#2: Not sure about this. I'll look into it. You can manually enter them in the .cfg file (i.e. you text-view)
#3: Yes.
Todd
Hi Todd,
Thank you for your answers. Your answers are very helpful.
Thanks,
Rahul