This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: waiting for root device while migrate from kernel 4.9 to kernel 4.19

Genius 13655 points

Part Number: AM5728
Other Parts Discussed in Thread: PMP, DRA752, TMP102

Hello Champs,

Customer failed to migrate from kernel 4.9 to kernel 4.19 (am57xx-evm-linux-sdk-src-06.03.00.106.tar.xz). 

It seems that the emmc isn't detected and the kernel is "waiting for root device", he has added the mmc driver in menuconfig. 

Below is the log.

BTW,  It can run on kernel 4.9.


U-Boot SPL 2017.01-g856bf87 (Aug 20 2020 - 16:05:07)
DRA752-GP ES2.0
Trying to boot from MMC2_2
reading u-boot.img
reading u-boot.img


U-Boot 2017.01-g856bf87 (Aug 20 2020 - 16:05:07 +0800)

CPU : DRA752-GP ES2.0
Board: Tronlong am57xx_evm boards
I2C: ready
DRAM: 1 GiB
WARNING: Caches not enabled
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit <SPACE> key to stop autoboot in 1s
Card did not respond to voltage select!
** Bad device mmc 0 **
There is no valid bmp file at the given address
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!
Trying to boot Linux from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
6394368 bytes read in 556 ms (11 MiB/s)
160698 bytes read in 28 ms (5.5 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffd5000, end 8ffff3b9 ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.94-gbe5389fd85 (root@qihua-virtual-machine) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11)) #2 SMP Tue Sep 13 15:12:58 CST 2022
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: TL5728-EasyEVM
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 80 MiB at 0x00000000bac00000
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to (ptrval) for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] random: get_random_bytes called from start_kernel+0xb4/0x460 with crng_init=0
[ 0.000000] percpu: Embedded 15 pages/cpu s32012 r8192 d21236 u61440
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 210240
[ 0.000000] Kernel command line: console=ttyO2,115200n8 omapdrm.displays=0,1 root=PARTUUID=9c1fae8a-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 575904K/847872K available (10240K kernel code, 321K rwdata, 2676K rodata, 2048K init, 273K bss, 26208K reserved, 245760K cma-reserved, 176128K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (12256 kB)
[ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB)
[ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 322 kB)
[ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 274 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] GIC: GICv2 detected, but range too small and irqchip.gicv2_force_probe not set
[ 0.000000] ti_dt_clocks_register: missing clkctrl nodes, please update your dts.
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000018] Switching to timer-based delay loop, resolution 162ns
[ 0.000356] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000366] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000849] Console: colour dummy device 80x30
[ 0.000868] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.000876] This ensures that you still see kernel messages. Please
[ 0.000883] update your kernel commandline.
[ 0.000914] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000928] pid_max: default: 32768 minimum: 301
[ 0.001049] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001063] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001612] CPU: Testing write buffer coherency: ok
[ 0.001648] CPU0: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulnerable
[ 0.001852] /cpus/cpu@0 missing clock-frequency property
[ 0.001869] /cpus/cpu@1 missing clock-frequency property
[ 0.001881] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002334] Setting up static identity map for 0x80200000 - 0x80200060
[ 0.002437] rcu: Hierarchical SRCU implementation.
[ 0.002786] EFI services will not be available.
[ 0.002917] smp: Bringing up secondary CPUs ...
[ 0.003515] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.003522] CPU1: Spectre v2: using ICIALLU workaround
[ 0.003637] smp: Brought up 1 node, 2 CPUs
[ 0.003648] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.003657] CPU: All CPU(s) started in HYP mode.
[ 0.003665] CPU: Virtualization extensions available.
[ 0.004150] devtmpfs: initialized
[ 0.028812] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.028985] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.029001] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.032966] pinctrl core: initialized pinctrl subsystem
[ 0.033459] DMI not present or invalid.
[ 0.033757] NET: Registered protocol family 16
[ 0.034821] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.035681] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.048137] omap_hwmod: mcasp3: no dt node
[ 0.048147] ------------[ cut here ]------------
[ 0.048169] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.048178] omap_hwmod: mcasp3: doesn't have mpu register target base
[ 0.048186] Modules linked in:
[ 0.048200] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.94-gbe5389fd85 #2
[ 0.048210] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.048217] Backtrace:
[ 0.048235] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.048247] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.048262] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.048275] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.048287] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.048298] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.048309] r8:00000000 r7:c1210cc4 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.048323] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.048331] r3:c0db3934 r2:c0db1b20
[ 0.048341] r6:c1204c48 r5:00000000 r4:c1210c8c
[ 0.048355] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.048366] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.048373] r4:c1210c8c
[ 0.048388] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.048397] r5:c12505c0 r4:c12505c0
[ 0.048412] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.048423] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.048438] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.048448] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.048455] r4:00000000
[ 0.048467] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.048475] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.048485] bfa0: 00000000 00000000 00000000 00000000
[ 0.048495] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.048505] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.048514] r5:c09fe3d0 r4:00000000
[ 0.048525] ---[ end trace 6cf6c81409687e58 ]---
[ 0.049379] omap_hwmod: mcasp4: no dt node
[ 0.049387] ------------[ cut here ]------------
[ 0.049400] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.049407] omap_hwmod: mcasp4: doesn't have mpu register target base
[ 0.049414] Modules linked in:
[ 0.049426] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.049434] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.049440] Backtrace:
[ 0.049453] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.049464] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.049475] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.049486] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.049496] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.049507] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.049517] r8:00000000 r7:c1210c48 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.049530] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.049538] r3:c0db3900 r2:c0db1b20
[ 0.049547] r6:c1204c48 r5:00000000 r4:c1210c10
[ 0.049561] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.049572] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.049579] r4:c1210c10
[ 0.049592] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.049601] r5:c12505c0 r4:c12505c0
[ 0.049614] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.049625] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.049639] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.049649] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.049656] r4:00000000
[ 0.049668] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.049676] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.049685] bfa0: 00000000 00000000 00000000 00000000
[ 0.049695] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.049704] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.049713] r5:c09fe3d0 r4:00000000
[ 0.049721] ---[ end trace 6cf6c81409687e59 ]---
[ 0.050584] omap_hwmod: mcasp5: no dt node
[ 0.050593] ------------[ cut here ]------------
[ 0.050607] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.050615] omap_hwmod: mcasp5: doesn't have mpu register target base
[ 0.050621] Modules linked in:
[ 0.050633] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.050641] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.050648] Backtrace:
[ 0.050661] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.050672] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.050683] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.050694] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.050704] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.050715] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.050726] r8:00000000 r7:c1210bcc r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.050739] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.050747] r3:c0db38cc r2:c0db1b20
[ 0.050756] r6:c1204c48 r5:00000000 r4:c1210b94
[ 0.050770] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.050781] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.050788] r4:c1210b94
[ 0.050801] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.050810] r5:c12505c0 r4:c12505c0
[ 0.050823] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.050834] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.050847] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.050858] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.050865] r4:00000000
[ 0.050877] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.050885] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.050894] bfa0: 00000000 00000000 00000000 00000000
[ 0.050903] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.050913] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.050921] r5:c09fe3d0 r4:00000000
[ 0.050929] ---[ end trace 6cf6c81409687e5a ]---
[ 0.051775] omap_hwmod: mcasp6: no dt node
[ 0.051783] ------------[ cut here ]------------
[ 0.051796] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.051803] omap_hwmod: mcasp6: doesn't have mpu register target base
[ 0.051810] Modules linked in:
[ 0.051822] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.051829] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.051836] Backtrace:
[ 0.051849] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.051859] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.051871] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.051882] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.051892] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.051902] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.051913] r8:00000000 r7:c1210b50 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.051925] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.051934] r3:c0db3898 r2:c0db1b20
[ 0.051943] r6:c1204c48 r5:00000000 r4:c1210b18
[ 0.051956] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.051967] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.051974] r4:c1210b18
[ 0.051987] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.051995] r5:c12505c0 r4:c12505c0
[ 0.052009] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.052020] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.052033] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.052044] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.052051] r4:00000000
[ 0.052062] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.052070] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.052079] bfa0: 00000000 00000000 00000000 00000000
[ 0.052089] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.052098] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.052107] r5:c09fe3d0 r4:00000000
[ 0.052114] ---[ end trace 6cf6c81409687e5b ]---
[ 0.052963] omap_hwmod: mcasp7: no dt node
[ 0.052970] ------------[ cut here ]------------
[ 0.052983] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.052991] omap_hwmod: mcasp7: doesn't have mpu register target base
[ 0.052997] Modules linked in:
[ 0.053009] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.053016] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.053023] Backtrace:
[ 0.053035] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.053045] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.053056] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.053067] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.053076] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.053087] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.053097] r8:00000000 r7:c1210ad4 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.053110] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.053118] r3:c0db3864 r2:c0db1b20
[ 0.053127] r6:c1204c48 r5:00000000 r4:c1210a9c
[ 0.053141] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.053151] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.053159] r4:c1210a9c
[ 0.053172] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.053180] r5:c12505c0 r4:c12505c0
[ 0.053193] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.053204] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.053217] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.053228] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.053235] r4:00000000
[ 0.053246] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.053254] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.053263] bfa0: 00000000 00000000 00000000 00000000
[ 0.053273] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.053282] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.053290] r5:c09fe3d0 r4:00000000
[ 0.053298] ---[ end trace 6cf6c81409687e5c ]---
[ 0.054152] omap_hwmod: mcasp8: no dt node
[ 0.054159] ------------[ cut here ]------------
[ 0.054173] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.054180] omap_hwmod: mcasp8: doesn't have mpu register target base
[ 0.054186] Modules linked in:
[ 0.054197] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.054205] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.054211] Backtrace:
[ 0.054224] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.054234] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.054245] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.054256] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.054266] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.054277] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.054287] r8:00000000 r7:c1210a58 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.054300] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.054309] r3:c0db3828 r2:c0db1b20
[ 0.054317] r6:c1204c48 r5:00000000 r4:c1210a20
[ 0.054331] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.054342] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.054349] r4:c1210a20
[ 0.054362] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.054370] r5:c12505c0 r4:c12505c0
[ 0.054384] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.054395] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.054408] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.054418] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.054425] r4:00000000
[ 0.054437] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.054445] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.054454] bfa0: 00000000 00000000 00000000 00000000
[ 0.054464] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.054473] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.054481] r5:c09fe3d0 r4:00000000
[ 0.054489] ---[ end trace 6cf6c81409687e5d ]---
[ 0.056107] omap_hwmod: dma_system: no dt node
[ 0.056115] ------------[ cut here ]------------
[ 0.056128] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.056136] omap_hwmod: dma_system: doesn't have mpu register target base
[ 0.056142] Modules linked in:
[ 0.056154] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.056161] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.056167] Backtrace:
[ 0.056180] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.056190] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.056201] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.056212] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.056221] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.056232] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.056242] r8:00000000 r7:c121274c r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.056255] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.056263] r3:c0db1eac r2:c0db1b20
[ 0.056272] r6:c1204c48 r5:00000000 r4:c1212714
[ 0.056286] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.056297] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.056304] r4:c1212714
[ 0.056318] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.056326] r5:c12505c0 r4:c12505c0
[ 0.056340] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.056351] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.056364] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.056375] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.056382] r4:00000000
[ 0.056393] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.056401] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.056410] bfa0: 00000000 00000000 00000000 00000000
[ 0.056420] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.056429] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.056438] r5:c09fe3d0 r4:00000000
[ 0.056445] ---[ end trace 6cf6c81409687e5e ]---
[ 0.071100] omap_hwmod: hdq1w: no dt node
[ 0.071109] ------------[ cut here ]------------
[ 0.071123] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.071131] omap_hwmod: hdq1w: doesn't have mpu register target base
[ 0.071138] Modules linked in:
[ 0.071151] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.071158] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.071165] Backtrace:
[ 0.071179] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.071190] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.071201] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.071212] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.071222] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.071234] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.071245] r8:00000000 r7:c12119e0 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.071259] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.071267] r3:c0db3b20 r2:c0db1b20
[ 0.071276] r6:c1204c48 r5:00000000 r4:c12119a8
[ 0.071290] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.071302] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.071309] r4:c12119a8
[ 0.071322] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.071331] r5:c12505c0 r4:c12505c0
[ 0.071345] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.071356] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.071369] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.071381] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.071389] r4:00000000
[ 0.071400] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.071409] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.071418] bfa0: 00000000 00000000 00000000 00000000
[ 0.071428] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.071437] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.071446] r5:c09fe3d0 r4:00000000
[ 0.071454] ---[ end trace 6cf6c81409687e5f ]---
[ 0.098339] omap_hwmod: smartreflex_core: no dt node
[ 0.098348] ------------[ cut here ]------------
[ 0.098362] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.098371] omap_hwmod: smartreflex_core: doesn't have mpu register target base
[ 0.098378] Modules linked in:
[ 0.098390] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.098398] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.098405] Backtrace:
[ 0.098419] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.098430] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.098442] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.098453] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.098464] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.098475] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.098486] r8:00000000 r7:c120fee8 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.098499] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.098508] r3:c0db3660 r2:c0db1b20
[ 0.098516] r6:c1204c48 r5:00000000 r4:c120feb0
[ 0.098530] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.098541] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.098549] r4:c120feb0
[ 0.098562] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.098570] r5:c12505c0 r4:c12505c0
[ 0.098584] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.098595] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.098609] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.098619] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.098626] r4:00000000
[ 0.098637] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.098646] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.098655] bfa0: 00000000 00000000 00000000 00000000
[ 0.098664] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.098674] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.098682] r5:c09fe3d0 r4:00000000
[ 0.098690] ---[ end trace 6cf6c81409687e60 ]---
[ 0.099533] omap_hwmod: smartreflex_mpu: no dt node
[ 0.099541] ------------[ cut here ]------------
[ 0.099554] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.099562] omap_hwmod: smartreflex_mpu: doesn't have mpu register target base
[ 0.099569] Modules linked in:
[ 0.099580] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.099587] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.099594] Backtrace:
[ 0.099608] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.099619] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.099630] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.099640] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.099651] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.099662] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.099673] r8:00000000 r7:c120fe74 r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.099686] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.099694] r3:c0db3650 r2:c0db1b20
[ 0.099703] r6:c1204c48 r5:00000000 r4:c120fe3c
[ 0.099717] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.099728] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.099735] r4:c120fe3c
[ 0.099748] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.099757] r5:c12505c0 r4:c12505c0
[ 0.099770] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.099781] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.099794] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.099805] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.099812] r4:00000000
[ 0.099823] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.099831] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.099840] bfa0: 00000000 00000000 00000000 00000000
[ 0.099850] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.099860] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.099869] r5:c09fe3d0 r4:00000000
[ 0.099876] ---[ end trace 6cf6c81409687e61 ]---
[ 0.128552] omap_hwmod: vip2: no dt node
[ 0.128561] ------------[ cut here ]------------
[ 0.128577] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2409 _init.constprop.26+0x1bc/0x4d4
[ 0.128585] omap_hwmod: vip2: doesn't have mpu register target base
[ 0.128593] Modules linked in:
[ 0.128605] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.19.94-gbe5389fd85 #2
[ 0.128614] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.128621] Backtrace:
[ 0.128635] [<c020bbd8>] (dump_backtrace) from [<c020bea8>] (show_stack+0x18/0x1c)
[ 0.128646] r7:00000009 r6:60000013 r5:00000000 r4:c124cedc
[ 0.128657] [<c020be90>] (show_stack) from [<c09e8d44>] (dump_stack+0x98/0xac)
[ 0.128669] [<c09e8cac>] (dump_stack) from [<c022dca0>] (__warn+0x104/0x11c)
[ 0.128679] r7:00000009 r6:c0db142c r5:00000000 r4:ef07bddc
[ 0.128690] [<c022db9c>] (__warn) from [<c022dd04>] (warn_slowpath_fmt+0x4c/0x68)
[ 0.128701] r8:00000000 r7:c1212e7c r6:6198b9f2 r5:c0db1b20 r4:c1204c48
[ 0.128714] [<c022dcbc>] (warn_slowpath_fmt) from [<c100d070>] (_init.constprop.26+0x1bc/0x4d4)
[ 0.128723] r3:c0db3da4 r2:c0db1b20
[ 0.128732] r6:c1204c48 r5:00000000 r4:c1212e44
[ 0.128746] [<c100ceb4>] (_init.constprop.26) from [<c100d4b8>] (__omap_hwmod_setup_all+0x48/0x134)
[ 0.128757] r10:00000003 r9:c1204c48 r8:ffffe000 r7:00000000 r6:c100d470 r5:c120a448
[ 0.128764] r4:c1212e44
[ 0.128778] [<c100d470>] (__omap_hwmod_setup_all) from [<c02025fc>] (do_one_initcall+0x5c/0x1a0)
[ 0.128787] r5:c12505c0 r4:c12505c0
[ 0.128801] [<c02025a0>] (do_one_initcall) from [<c1000ff8>] (kernel_init_freeable+0x1d4/0x26c)
[ 0.128812] r9:c1000620 r8:000000da r7:c1050824 r6:c1064800 r5:c12505c0 r4:c12505c0
[ 0.128826] [<c1000e24>] (kernel_init_freeable) from [<c09fe3e0>] (kernel_init+0x10/0x118)
[ 0.128836] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09fe3d0
[ 0.128843] r4:00000000
[ 0.128855] [<c09fe3d0>] (kernel_init) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 0.128863] Exception stack(0xef07bfb0 to 0xef07bff8)
[ 0.128872] bfa0: 00000000 00000000 00000000 00000000
[ 0.128881] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.128891] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.128899] r5:c09fe3d0 r4:00000000
[ 0.128907] ---[ end trace 6cf6c81409687e62 ]---
[ 0.217452] cpuidle: using governor ladder
[ 0.217488] cpuidle: using governor menu
[ 0.223991] OMAP GPIO hardware version 0.1
[ 0.228347] OF: /ocp/serial@4806c000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core_aon@5000/clocks/atl_clkin2_ck
[ 0.228598] OF: /ocp/serial@48020000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core_aon@5000/clocks/atl_clkin1_ck
[ 0.228862] OF: /ocp/serial@4806e000: could not get #interrupt-cells for /ocp/l4@4ae00000/prm@6000/clocks/abe_sys_clk_div@120
[ 0.229113] OF: /ocp/serial@48066000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core@8000/clocks/dpll_per_m2_ck@150
[ 0.229368] OF: /ocp/serial@48068000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core_aon@5000/clocks/usb_dpll_hs_clk_div
[ 0.229622] OF: /ocp/serial@48420000: could not get #interrupt-cells for /ocp/l4@4a000000/scm@2000/pinmux@1400/i2c2_pins_default
[ 0.229876] OF: /ocp/serial@48422000: could not get #interrupt-cells for /ocp/l4@4a000000/scm@2000/pinmux@1400/i2c3_pins_default
[ 0.230157] OF: /ocp/serial@48424000: could not get #interrupt-cells for /ocp/l4@4a000000/scm@2000/pinmux@1400/i2c5_pins_default
[ 0.249060] No ATAGs?
[ 0.249156] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.249172] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.249204] omap_device: omap_dma_system: build failed (-22)
[ 0.249214] omap2_system_dma_init_dev: Can't build omap_device for omap_dma_system:dma_system.
[ 0.260463] edma 43300000.edma: memcpy is disabled
[ 0.263769] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.267893] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.268058] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.268280] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.268510] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.268873] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.269028] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.269278] iommu: Adding device 58820000.ipu to group 1
[ 0.269355] iommu: Adding device 55020000.ipu to group 2
[ 0.269465] iommu: Adding device 40800000.dsp to group 0
[ 0.269690] iommu: Adding device 41000000.dsp to group 3
[ 0.270940] SCSI subsystem initialized
[ 0.271103] usbcore: registered new interface driver usbfs
[ 0.271151] usbcore: registered new interface driver hub
[ 0.271211] usbcore: registered new device driver usb
[ 0.272047] palmas 0-0058: Irq flag is 0x00000008
[ 0.302874] palmas 0-0058: Muxing GPIO 2b, PWM 0, LED 0
[ 0.305023] SMPS12: supplied by regulator-dummy
[ 0.306594] SMPS3: supplied by regulator-dummy
[ 0.306926] smps3: Bringing 1500000uV into 1350000-1350000uV
[ 0.308882] SMPS45: supplied by regulator-dummy
[ 0.309227] smps45: Bringing 1170000uV into 1060000-1060000uV
[ 0.311278] SMPS6: supplied by regulator-dummy
[ 0.312830] SMPS7: supplied by regulator-dummy
[ 0.314302] random: fast init done
[ 0.314559] SMPS8: supplied by regulator-dummy
[ 0.315720] SMPS9: supplied by regulator-dummy
[ 0.316362] LDO1: supplied by regulator-dummy
[ 0.324418] LDO2: supplied by regulator-dummy
[ 0.334295] LDO3: supplied by regulator-dummy
[ 0.344306] LDO4: supplied by regulator-dummy
[ 0.354329] LDO5: supplied by regulator-dummy
[ 0.354969] LDO6: supplied by regulator-dummy
[ 0.355609] LDO7: supplied by regulator-dummy
[ 0.356244] LDO8: supplied by regulator-dummy
[ 0.356896] LDO9: supplied by regulator-dummy
[ 0.364350] LDOLN: supplied by regulator-dummy
[ 0.374372] LDOUSB: supplied by regulator-dummy
[ 0.386574] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.387148] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.387379] media: Linux media interface: v0.10
[ 0.387418] videodev: Linux video capture interface: v2.00
[ 0.387489] pps_core: LinuxPPS API ver. 1 registered
[ 0.387498] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.387518] PTP clock support registered
[ 0.387547] EDAC MC: Ver: 3.0.0
[ 0.388265] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 0.388503] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 0.388731] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.388953] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.389299] Advanced Linux Sound Architecture Driver Initialized.
[ 0.390060] clocksource: Switched to clocksource arch_sys_counter
[ 0.397591] NET: Registered protocol family 2
[ 0.398120] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
[ 0.398149] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.398212] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.398338] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.398408] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.398442] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.398568] NET: Registered protocol family 1
[ 0.398934] RPC: Registered named UNIX socket transport module.
[ 0.398944] RPC: Registered udp transport module.
[ 0.398953] RPC: Registered tcp transport module.
[ 0.398960] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.399935] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.400151] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.401102] Initialise system trusted keyrings
[ 0.401224] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.405946] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.406388] NFS: Registering the id_resolver key type
[ 0.406410] Key type id_resolver registered
[ 0.406419] Key type id_legacy registered
[ 0.406458] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.408067] Key type asymmetric registered
[ 0.408079] Asymmetric key parser 'x509' registered
[ 0.408125] bounce: pool size: 64 pages
[ 0.408157] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.408168] io scheduler noop registered
[ 0.408177] io scheduler deadline registered
[ 0.408269] io scheduler cfq registered (default)
[ 0.408279] io scheduler mq-deadline registered
[ 0.408288] io scheduler kyber registered
[ 0.411159] phy phy-4a084000.phy.0: Linked as a consumer to regulator.22
[ 0.411426] phy phy-4a085000.phy.1: Linked as a consumer to regulator.22
[ 0.413603] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[ 0.417669] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.3
[ 0.417856] dra7-pcie 51000000.pcie: WA for Errata i870 not applied
[ 0.417939] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 0.417955] dra7-pcie 51000000.pcie: No bus range found for /ocp/axi@0/pcie@51000000, using [bus 00-ff]
[ 0.417990] dra7-pcie 51000000.pcie: IO 0x20003000..0x20012fff -> 0x00000000
[ 0.418020] dra7-pcie 51000000.pcie: MEM 0x20013000..0x2fffffff -> 0x20013000
[ 1.418299] dra7-pcie 51000000.pcie: Phy link never came up
[ 1.418429] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 1.418443] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.418455] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.418466] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.425119] PCI: bus0: Fast back to back transfers disabled
[ 1.431318] PCI: bus1: Fast back to back transfers enabled
[ 1.431359] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
[ 1.431379] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 1.431687] pcieport 0000:00:00.0: Signaling PME with IRQ 195
[ 1.431814] pcieport 0000:00:00.0: AER enabled with IRQ 195
[ 1.432948] pwm-backlight backlight: backlight supply power not found, using dummy regulator
[ 1.433020] pwm-backlight backlight: Linked as a consumer to regulator.0
[ 1.435695] vdd_3v3: supplied by regen1
[ 1.435923] aic_dvdd_fixed: supplied by vdd_3v3
[ 1.435981] vtt_fixed: supplied by smps3
[ 1.480348] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 1.483024] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 45, base_baud = 3000000) is a 8250
[ 1.483305] OF: /ocp/serial@4806c000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core_aon@5000/clocks/atl_clkin2_ck
[ 1.483841] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 46, base_baud = 3000000) is a 8250
[ 1.484107] OF: /ocp/serial@48020000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core_aon@5000/clocks/atl_clkin1_ck
[ 1.484614] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 47, base_baud = 3000000) is a 8250
[ 5.231444] console [ttyS2] enabled
[ 5.235231] OF: /ocp/serial@4806e000: could not get #interrupt-cells for /ocp/l4@4ae00000/prm@6000/clocks/abe_sys_clk_div@120
[ 5.247129] 4806e000.serial: ttyS3 at MMIO 0x4806e000 (irq = 48, base_baud = 3000000) is a 8250
[ 5.256161] OF: /ocp/serial@48066000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core@8000/clocks/dpll_per_m2_ck@150
[ 5.268313] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 49, base_baud = 3000000) is a 8250
[ 5.277346] OF: /ocp/serial@48068000: could not get #interrupt-cells for /ocp/l4@4a000000/cm_core_aon@5000/clocks/usb_dpll_hs_clk_div
[ 5.289936] 48068000.serial: ttyS5 at MMIO 0x48068000 (irq = 50, base_baud = 3000000) is a 8250
[ 5.298965] OF: /ocp/serial@48420000: could not get #interrupt-cells for /ocp/l4@4a000000/scm@2000/pinmux@1400/i2c2_pins_default
[ 5.311133] 48420000.serial: ttyS6 at MMIO 0x48420000 (irq = 51, base_baud = 3000000) is a 8250
[ 5.320152] OF: /ocp/serial@48422000: could not get #interrupt-cells for /ocp/l4@4a000000/scm@2000/pinmux@1400/i2c3_pins_default
[ 5.332313] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 52, base_baud = 3000000) is a 8250
[ 5.341324] OF: /ocp/serial@48424000: could not get #interrupt-cells for /ocp/l4@4a000000/scm@2000/pinmux@1400/i2c5_pins_default
[ 5.353492] 48424000.serial: ttyS8 at MMIO 0x48424000 (irq = 53, base_baud = 3000000) is a 8250
[ 5.363032] 4ae2b000.serial: ttyS9 at MMIO 0x4ae2b000 (irq = 54, base_baud = 3000000) is a 8250
[ 5.373797] omap_rng 48090000.rng: Random Number Generator ver. 20
[ 5.374261] random: crng init done
[ 5.384021] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 5.391155] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 5.406696] brd: module loaded
[ 5.415755] loop: module loaded
[ 5.447299] ti-qspi 4b300000.qspi: No Rx DMA available, trying mmap mode
[ 5.455288] libphy: Fixed MDIO Bus: probed
[ 5.462189] dwc3 48890000.usb: Failed to get clk 'ref': -2
[ 5.470374] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.475907] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 5.483869] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
[ 5.493359] xhci-hcd xhci-hcd.0.auto: irq 197, io mem 0x48890000
[ 5.500214] hub 1-0:1.0: USB hub found
[ 5.504018] hub 1-0:1.0: 1 port detected
[ 5.508277] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.513820] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 5.521534] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 5.528188] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 5.536900] hub 2-0:1.0: USB hub found
[ 5.540718] hub 2-0:1.0: 1 port detected
[ 5.545067] usbcore: registered new interface driver usb-storage
[ 5.580314] rtc-ds1307: probe of 3-006f failed with error -121
[ 5.586212] i2c /dev entries driver
[ 5.591809] tmp102 0-0048: error reading config register
[ 5.597230] tmp102: probe of 0-0048 failed with error -121
[ 5.603770] cpu cpu0: "syscon" is missing, cannot use OPPv2 table.
[ 5.611136] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 5.619964] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 5.624851] omap_hsmmc 4809c000.mmc: RX DMA channel request failed
[ 5.631777] omap_hsmmc 480b4000.mmc: RX DMA channel request failed
[ 5.639531] ledtrig-cpu: registered to indicate activity on CPUs
[ 5.648653] NET: Registered protocol family 10
[ 5.653882] Segment Routing with IPv6
[ 5.657621] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 5.664054] NET: Registered protocol family 17
[ 5.668713] Key type dns_resolver registered
[ 5.673163] Registering SWP/SWPB emulation handler
[ 5.677978] omap_voltage_late_init: Voltage driver support not added
[ 5.684374] Power Management for TI OMAP4+ devices.
[ 5.689971] Loading compiled-in X.509 certificates
[ 5.710785] dmm 4e000000.dmm: failed to initialize work-around for i878
[ 5.718916] dmm 4e000000.dmm: initialized all PAT entries
[ 5.725931] omap_i2c 48072000.i2c: bus 1 rev0.12 at 100 kHz
[ 5.732388] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
[ 5.738477] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 5.745603] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 5.753352] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 5.760441] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 5.768207] hctosys: unable to open rtc device (rtc0)
[ 5.774115] ALSA device list:
[ 5.777097] No soundcards found.
[ 5.781194] Waiting for root device PARTUUID=9c1fae8a-02...
[ 5.900077] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 6.136292] hub 1-1:1.0: USB hub found
[ 6.140137] hub 1-1:1.0: 4 ports detected
[ 6.201292] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 6.208374] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 6.230124] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
[ 6.280275] hub 2-1:1.0: USB hub found
[ 6.284100] hub 2-1:1.0: 4 ports detected
[ 6.291385] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 6.298444] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 6.520075] usb 1-1.1: new high-speed USB device number 3 using xhci-hcd
[ 6.714909] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 6.722174] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 6.820074] usb 1-1.2: new high-speed USB device number 4 using xhci-hcd
[ 7.002918] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 7.009983] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 7.110077] usb 1-1.3: new high-speed USB device number 5 using xhci-hcd
[ 7.290923] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 7.297977] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 7.400078] usb 1-1.4: new high-speed USB device number 6 using xhci-hcd
[ 7.578919] omapdss_dss 58000000.dss: Linked as a consumer to regulator.21
[ 7.586000] omapdss_dss 58000000.dss: Dropping the link to regulator.21
[ 36.330089] aic_dvdd_fixed: disabling
[ 36.333774] vmmcwl_fixed: disabling
[ 36.337299] pbias_mmc_omap5: disabling

Thanks
Rgds
Shine