This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

audio gadget failed, need help



Hi, 

Need help on MCASP ALSA driver,

1. could not output 24/32bit  sound, all clipped to 16bit. where could I correct this error? I have no clue where the data transfer to the FIFO code is( I need to know the data path of the data from user to XBUF). below is the output by aplay

 

Playing WAVE '/media/mmcblk0p1/test192k.wav' : Signed 24 bit Little Endian in 3bytes, Rate 192000 Hz, Stereo

params_format(params):10  ------------------ means 32 bit output

channel size word:5   

 

 

2. and, insmod g_audio.ko, in windows side, 

The device cannot start (code 10)

don't know what's wrong with this module.

 

3. wanna use DIT mode, how to configure the kernel/hardware?

 

Best regards,

Power Pan