Part Number: TDA4VM
Hi team,
I configure GPIO for this, but it can't work right.
gpio0_21 input
GPIO_PinConfig gpioPinConfigs[] = {
GPIO_DEVICE_CONFIG(0, 21) | GPIO_CFG_INPUT | GPIO_CFG_IN_INT_RISING
};
/* GPIO Driver call back functions */
GPIO_CallbackFxn gpioCallbackFunctions[] = {
NULL
};
/* GPIO Driver configuration structure */
GPIO_v0_Config GPIO_v0_config = {
gpioPinConfigs,
gpioCallbackFunctions,
sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig),
sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn),
0,
};
uint32_t cnt = 0;
void AppGpioCallbackFxn(void)
{
cnt++;
}
static void GPIO_configIntRouter(uint32_t portNum, uint32_t pinNum, uint32_t gpioIntRtrOutIntNum, GPIO_v0_HwAttrs *cfg)
{
GPIO_IntCfg *intCfg;
uint32_t bankNum = 0U;
intCfg = cfg->intCfg;
cfg->baseAddr = 0x600000UL;
bankNum = pinNum/16; /* Each GPIO bank has 16 pins */
intCfg[pinNum].intNum = 176 + bankNum; //CSLR_R5FSS1_CORE0_INTR_GPIOMUX_INTRTR0_OUTP_16
intCfg[pinNum].intcMuxNum = INVALID_INTC_MUX_NUM;
intCfg[pinNum].intcMuxInEvent = 0;
intCfg[pinNum].intcMuxOutEvent = 0;
}
set RmIrq ,I'm not sure if it's right
static void SetRmIrqGPIO()
{
struct tisci_msg_rm_irq_set_req rmIrqReq;
struct tisci_msg_rm_irq_set_resp rmIrqResp;
memset(&rmIrqReq, 0x0, sizeof(rmIrqReq));
memset(&rmIrqResp, 0x0, sizeof(rmIrqResp));
rmIrqReq.valid_params = 0U;
rmIrqReq.global_event = 0U;
rmIrqReq.src_id = 0U;
rmIrqReq.src_index = 0U;
rmIrqReq.dst_id = 0U;
rmIrqReq.dst_host_irq = 0U;
rmIrqReq.ia_id = 0U;
rmIrqReq.vint = 0U;
rmIrqReq.vint_status_bit_index = 0U;
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
rmIrqReq.src_id = 105; //TISCI_DEV_GPIOMUX_INTRTR0;
rmIrqReq.src_index = 21; //Need to add 128 for GPIO1
/* Set the destination based on the core */
rmIrqReq.dst_id = 247; //TISCI_DEV_R5FSS1_CORE0;
rmIrqReq.dst_host_irq = 257; //don't know how to set this
/* Set the destination interrupt */
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_ID_VALID;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID;
Sciclient_rmIrqSet(
(const struct tisci_msg_rm_irq_set_req *)&rmIrqReq,
&rmIrqResp,
SCICLIENT_SERVICE_WAIT_FOREVER);
}
void AppGpioCallbackFxn(void)
{
cnt++;
}
static void appMain(void* arg0, void* arg1)
{
GPIO_v0_HwAttrs gpio_cfg;
uint8_t flag = 0;
Board_initCfg boardCfg;
boardCfg = BOARD_INIT_UART_STDIO ;//| BOARD_INIT_PINMUX_CONFIG| BOARD_INIT_MODULE_CLOCK;
Board_init(boardCfg);
appInit();
appRun();
Osal_delay(10000);
GPIO_socGetInitCfg(0, &gpio_cfg); //
gpio_cfg.baseAddr = 0x600000UL;
GPIO_configIntRouter(0, 21, 0, &gpio_cfg);
*(volatile uint32_t *)0x00011C058 = 0x0050007;
GPIO_socSetInitCfg(0, &gpio_cfg);
SetRmIrqGPIO();
GPIO_init();
GPIO_setCallback(0, AppGpioCallbackFxn);
GPIO_enableInt(0);
while(1)
{
flag = GPIO_read(0);
UART_printf("cnt: %d, %d\n", flag, cnt);
appLogWaitMsecs(100u);
}
}
after set this,I gave a 100Hz PWM pulse to GPIO0_21, I try to printf the value of cnt, but the value of cnt is always 0,
and GPIO_read(0) can get change of GPIO.
Can you tell me what is wrong with my configuration?
and I want to know how to set these parameter?
rmIrqReq.src_id
rmIrqReq.src_index
rmIrqReq.dst_id
rmIrqReq.dst_host_irq