This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6486 power consumption

To whom might concern,

When I tried to run while loop, TCI6486 power consumption was increasing and higher than any tasking like: SRIO, EMAC or EDMA.

Does anyone can tell me why?

 

Sincerely,

SUNGYI CHEN

 

 

 

 

  • It's possible that some amount of self heating which will increase the temperature of the device resulting in an increase of leakage current \resulting in the power consumption increasing over time as the device heats up.  It would reach a steady state at some point.

    When observing the other IP usage on SRIO, EMAC, etc was it at the same case temperature and the same device?

    Best Regards,

    Chad Courtney