Part Number: 66AK2G12
Hi,
I am writing some fairly simple code running on the C66 core only and have hit a brick wall when trying to get interrupts in place. I am writing the code bare metal and not using an RTOS or SDK.
I can confirm that I have the UART Rx interrupt enabled and that the pending flags are set when a char is Rx'ed. I think I have the CIC set up, but cannot be 100% certain as the ref manual is not very clear how this section is meant to work. I feel that there is a section I am missing: I am trying to read up on the interrupts for the C66 core, but am not getting very far as all the manuals/datasheets/guides seems to reference each other without any of them actually explaining how the interrupts work!
Do you have a simple code example I could follow?
Many thanks, Todd