Other Parts Discussed in Thread: SYSBIOS
I'm attempting to build some C674 code in CCS using DMAN3 and ACPY3 and I'm getting the following error:
error: xdc.runtime.knl.SemProcess: "C:/TexasInstruments/xdctools_3_20_08_88/packages/xdc/runtime/knl/SemProcess.xs", line 28: xdc.runtime.knl.SemProcess : SemProcess.Proxy is not bound to OS specific implementation
js: "C:/TexasInstruments/xdctools_3_20_08_88/packages/xdc/cfg/Main.xs", line 116: Error: Configuration failed!
xdctools_3_20_08_88\gmake.exe: *** [package/cfg/DSPtasks_ti81xx_dsp_p674.xdl] Error 1
js: "C:/TexasInstruments/xdctools_3_20_08_88/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: *** [configPkg/compiler.opt] Error 1
gmake: Target `all' not remade because of errors.
Build complete for project DSPtasks_CCS4
The .cfg file appears to be the source of the error:
DSPtasks_ti816x_dsp.cfg:
/* Set the BIOS timer frequency to 32KHz so as to match with the default timer
* frequency on Linux
*/
var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
Timer.intFreq.hi = 0;
Timer.intFreq.lo = 32768;
var System = xdc.useModule('xdc.runtime.System');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.setConfig("DSP", ["DSP", "VIDEO-M3", "VPSS-M3", "HOST"]);
/* Load common configuration needed for running all SysLink samples */
xdc.loadCapsule("DSPtasks_common.cfg.xs");
var Notify = xdc.useModule('ti.sdo.ipc.Notify');
var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ');
var GateMP = xdc.useModule('ti.sdo.ipc.GateMP');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Sem = xdc.useModule('ti.sysbios.knl.Semaphore');
var Memory = xdc.useModule('xdc.runtime.Memory');
Memory.defaultHeapSize = 0x8000;
Program.heap = 0x8000;
// Place heaps. L1DSRAM is defined in platform file
Program.sectMap[".L1D_HEAP"] = "L1DSRAM"; // L1DHEAP
Program.sectMap[".EXTERNAL_HEAP"] = "DDR2"; // EXTERNALHEAP
Program.sectMap[".text"] = "DDR2";
/* Task that does the message passing */
var tsk1 = Task.create('&Preprocessing_taskFxn');
tsk1.instance.name = "Preprocessing_taskFxn";
tsk1.arg0 = MultiProc.getIdMeta ("HOST");
tsk1.stackSize = 0x1000;
/* DMAN3 stuff */
var DMAN3 = xdc.useModule('ti.sdo.fc.dman3.DMAN3');
DMAN3.heapInternal = ".L1D_HEAP";
DMAN3.heapExternal = ".EXTERNAL_HEAP";
/* ACPY3 stuff */
var ACPY3 = xdc.useModule('ti.sdo.fc.acpy3.ACPY3');
DSPtasks_common.cfg.xs:
var Ipc = xdc.useModule('ti.sdo.ipc.Ipc');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
var Syslink = xdc.useModule ('ti.syslink.ipc.rtos.Syslink');
xdc.loadPackage ('ti.syslink.ipc.rtos');
if ( (Program.platform.$name != undefined) && (Program.platform.$name.match(/evmDA830/)) ) {
/* Ipc */
Ipc.sr0MemorySetup = true;
}
/* Ipc configuration */
if ( (Program.platform.$name != undefined) && (Program.platform.$name.match(/evm6472/)) ) {
/* Set host id */
Ipc.hostProcId = MultiProc.getIdMeta("CORE5");
Ipc.generateSlaveDataForHost = true;
}
else if ( (Program.platform.$name != undefined) && (Program.platform.$name.match(/evm6474/)) ) {
/* Set host id */
Ipc.hostProcId = MultiProc.getIdMeta("CORE2");
Ipc.generateSlaveDataForHost = true;
}
else {
/* Set host id */
Ipc.hostProcId = MultiProc.getIdMeta("HOST");
}
Ipc.procSync = Ipc.ProcSync_PAIR;
/* Set Shared Region variables by picking up the information from Platform
* memory map
*/
var sr0MemSection = Program.cpu.memoryMap['SR0'];
/*
var SHAREDREG_0_MEM = sr0MemSection.base;
var SHAREDREG_0_MEMSIZE = sr0MemSection.len;
*/
var SHAREDREG_0_MEM = 0x97600000;
var SHAREDREG_0_MEMSIZE = 0x10000000;
var SHAREDREG_0_ENTRYID = 0;
var SHAREDREG_0_OWNERPROCID = Ipc.hostProcId;
var sr1MemSection = Program.cpu.memoryMap['SR1'];
/*
var SHAREDREG_1_MEM = sr1MemSection.base;
var SHAREDREG_1_MEMSIZE = sr1MemSection.len;
*/
var SHAREDREG_1_MEM = 0x96A00000;
var SHAREDREG_1_MEMSIZE = 0x00C00000;
var SHAREDREG_1_ENTRYID = 1;
var SHAREDREG_1_OWNERPROCID = Ipc.hostProcId;
/*
* Need to define the shared region. The IPC modules use this
* to make portable pointers. All processors need to add this
* call with their base address of the shared memory region.
* If the processor cannot access the memory, do not add it.
*/
SharedRegion.setEntryMeta(SHAREDREG_0_ENTRYID,
{
base: SHAREDREG_0_MEM,
len: SHAREDREG_0_MEMSIZE,
ownerProcId: SHAREDREG_0_OWNERPROCID,
isValid: true,
name: "shared_region_0",
});
SharedRegion.setEntryMeta(SHAREDREG_1_ENTRYID,
{
base: SHAREDREG_1_MEM,
len: SHAREDREG_1_MEMSIZE,
ownerProcId: SHAREDREG_1_OWNERPROCID,
isValid: true,
name: "shared_region_1",
createHeap: true
});
/*
* Application constants that all three programs use.
*/
Program.global.MSGQ_NAME = "MSGQ_";
Program.global.HEAP_NAME = "HeapMemMP";
Program.global.HEAP_ALIGN = 128;
Program.global.HEAP_MSGSIZE = 128;
Program.global.HEAP_NUMMSGS = 10;
Program.global.HEAPID = 0;
Update:
The error is apparently coming from the inclusion of:
var ACPY3 = xdc.useModule('ti.sdo.fc.acpy3.ACPY3')
in DSPtasks_ti816x_dsp.cfg file.
Update Secundum:
I got rid of the error by inserting the following two lines in the common part of the .cfg:
var SemProcess = xdc.useModule('xdc.runtime.knl.SemProcess');
SemProcess.Proxy = xdc.useModule('ti.sysbios.xdcruntime.SemProcessSupport');
I'm not sure why I needed to do this.
Lee Holeva