Part Number: TDA4VM-Q1
Hi team,
Here's an issue from the customer may need your help:
During debug, when using MMA for FFT, the CPU voltage rail has a sudden change in current.
The peak current is around 4A maximum, and the 3 bucks together have a peak current of 12A, which is much higher than the sum of the PMIC 3 Phase bucks. Occasionally CPU downtime occurs and the PMIC buck does not have any voltage output. So the customer has the following questions:
- Does TI test the data for the power consumption of the MMA? What are the data results?
- How to fix the issue above?
- Which modules are powered by the two voltages of the CPU core?
- Does the use of the MMA primarily cause current to increase in the CPU voltage rail or is it affected by both?
Could you help check this case? Thanks.
Best Regards,
Cherry