Hi,
I did not find any sd card included on my
J721EXCP01EVM and
J7200XSOMG01EVM
So I created one using instructions from software-dl.ti.com/.../Processor_SDK_Linux_Formatting_SD_Card.html.
Now I have almost the same setup as the related thread except for the som (J7200XSOMG01EVM), needed files are on boot and rootfs partition, dip switches are set to boot from sd but still
experiencing the same problem. I understand that the potential solution is to reset som; does that mean pressing the blue button on it as shown on the attached image (I still can't boot from the sd card after I did that).
thanks,
wbb
![]()