Other Parts Discussed in Thread: AM3517
Dear All ! I have downloaded the Kernel source from GIT source tree for RTLINux but it gives error at the end of compilation. mm/highmem.c: In function 'pkmap_try_free': mm/highmem.c:121:17: warning: unused variable 'addr' mm/highmem.c: In function 'kmap_high_get': mm/highmem.c:425:2: error: 'kmap_lock' undeclared (first use in this function) mm/highmem.c:425:2: note: each undeclared identifier is reported only once for each function it appears in make[1]: *** [mm/highmem.o] Error 1 make: *** [mm] Error 2 Thanks and regards hrishikesh