Other Parts Discussed in Thread: AM1705
Our minimal requirements are next:
1. QFP body, not BGA
2. NAND interface for flash (to use single large NAND flash IC instead of number of ICs (for example - on 1705 - we can use 3 NOR ICs with 32M space, not one NOR with 128M))
3. SDRAM interface for RAM (needed to run OS)
4. One Ethernet / MAC
5. One USB
6. Three UARTs
7. Linux OS (for using different applications in energy monitoring and accounting systems)
Please help us to choise some TI devices?
With Regards.