This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC110: EtherCAT can't reach 500us cycle time

Part Number: AMIC110


Hello Sirs,

I've developing project using AMIC110 and EtherCAT slave stack code with TI-RTOS,

I've use TwinCAT2 and Bechoff controller and try to configure the cycle time to 500us 

but it will last reach err-safeop and return error code 0x001a (synchronization error)(1ms and above is fine)

As I trace the slave stack code, the state machine watchdog has expired so it return error code 0x001a

Is there any way to investigate the reason time-out reached? and how to solve this issue?


Thanks a lot!