This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c5515: porting ccs3.3 project into ccs4



after porting my project from ccs3.3 to ccs4 I'm getting the bellow linking remark:

"/.fpcnf.cmd...  .printf is not allocated, but is being placed as part of allocated object "GROUP_1"

how can I remove this remark?  

  • Talmor,

    I'm going to need a few more things from you to help you out.

    1) Is /".fpcnf.cmd... .printf" part of your code or are you trying to link this from a library?

    2) When you converted your project, did you create it under a subfolder of the original project? If so, you might need to add the original project's library and include under the new project.

    Regards,

    Juliana Almeida

  • Hi Juliana,

    1. yes it's part of my project and i think this file was created automatically .

    2. no , I jus imported it as a Legacy cc3.3 project

    Thanks for ypur help

    Talmor

  • Juliana

    I'm also getting the bellow error when trying to work with the debuger:

    "ROV failed to start....There is a version mismatch between the ROV server and the ROV plug in . Make suere the most recent VDC tools version is selected."

    Can you please help me with that ?

    Thanks

    Talmor

     

  • I tried to use the "printf" function in my code and I'm getting the following linking errors:

    <Linking>

    "C:/G10/./fpcfg.cmd", line 290: remark: object ".printf" is not allocated, but

    "C:/G10/./fpcfg.cmd", line 326: error: run placement fails for object ".pip",

    is being placed as part of allocated object "GROUP_1"

    size 0xc8 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x154 max hole: 0x84

    "C:/G10/./fpcfg.cmd", line 207: error: run placement fails for object ".tsk",

    size 0xb8 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x154 max hole: 0x84

    "C:/G10/./fpcfg.cmd", line 331: error: run placement fails for object ".sts",

    size 0x90 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x154 max hole: 0x84

    "C:/G10/./fpcfg.cmd", line 250: error: placement fails for object ".switch",

    size 0x20 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x22 max hole: 0x12

    "C:/G10/./fpcfg.cmd", line 214: error: run placement fails for object ".idl",

    size 0x10 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 218: error: run placement fails for object

    ".idlcal", size 0x10 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 264: error: run placement fails for object ".sys",

    size 0x10 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 268: error: placement fails for object ".pinit",

    size 0xc (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 305: error: placement fails for object ".args", size

    0x8 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 167: error: run placement fails for object ".clk",

    size 0x8 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 254: error: placement fails for object ".trcdata",

    size 0x6 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x12 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 198: error: run placement fails for object ".swi",

     

    size 0x50 (page 0). Available ranges:

    >> Compilation failure

    DARAM size: 0xfe40 unused: 0x10 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 316: error: run placement fails for object ".hst",

    size 0x34 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x10 max hole: 0x4

    "C:/G10/./fpcfg.cmd", line 321: error: run placement fails for object ".log",

    size 0x28 (page 0). Available ranges:

    DARAM size: 0xfe40 unused: 0x10 max hole: 0x4

    error: errors encountered during linking; "C:/G10/Debug/fp.out" not built

    C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: *** [C:/G10/Debug/fp.out] Error 1

    C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.

     

    Need help ....

     

     

     

     

  • About yout ROV failed to start error, check out this thread:

    http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/36934/128994.aspx

    See if that fixes your errors.

     

    Regards,

    Juliana Almeida

  • what about the "printf" issue . any idea how can I allocate space for printf and solve the following linker issue:

    "".printf" is not allocated, but is being placed as part of allocated object "GROUP_1"

    BR

    Talmor