This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: AM6234

Part Number: PROCESSOR-SDK-AM62X


I’m looking at the OLDI LVDS interface on the TI AM6234. I couldn’t find the LVDS interface specs in the datasheet. I attempted to find the interface characteristic information on this forum but the closest I found was this thread which didn’t include interface's characteristics. 

 

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1131079/sk-am62-lvds-is-1-8v-interface-in-am62x-can-i-use-a-3-3-v-lcd-panel-directly

 

The AM6234 display’s LVDS power rail is 1.8V, so I'm assuming the OLDI output is LVDS at 1.8V.

I want to directly attach my LVDS 3.3V display to the AM6234.

Since it’s LVDS, as long as the common mode range and the differential voltage swing is compatible between the two devices there will be no problem and I can DC couple the interface. The common mode voltage is 1.2V and the differential voltage swing is between 0.2V and 0.6V.

Please post the LVDS interface characteristics