Hi
I have a question regarding the GPTIMERs on AM3517 under Linux.
I'm writing a PWM driver for Linux that use GPTIMER10 for PWM generation by default the timer is setup to use the 32kHz as the clock source.
How do I change the clock source from the 32kHz to the system clock in my driver code?
I'm using the Linux source from AM35x-OMAP35x-PSP-04.02.00.07.
Best regards,
Anders