Hi,
I am working on a new design for a board with a DM642 processor and an on-board Ethernet switch. Since the switch is on the same board as the DM642, we can connect the DM642 directly to the switch, with no PHY in between. I am wondering how the NDK would be affected by this configuration. Will the stack still work if it does not detect (via the MDIO interface) that a connection has been made to the (in this case non-existent) PHY? Will I have to rebuild the NDK to remove the code that tries to talk to the PHY?
Any help on this would be greatly appreciated.
Paul