Hello,
We are seeing the following error message during booting. Do you have any suggestions on what the issue(s) may be? We are seeing it on 2 (of 2) of the latest boards and did not see it on previous EVMs.
Thank you,
Gary
- 2 new Centaurus EVM have the same error.
ata1: irq_stat 0x00000040, connection status changed
ata1: SError: { DevExch }
ata1: limiting SATA link speed to 1.5 Gbps
ata1: hard resetting link
ata1: SATA link down (SStatus 0 SControl 310)
ata1: EH complete
ata1: exception Emask 0x10 SAct 0x0 SErr 0x4000000 action 0xe frozen
ata1: irq_stat 0x00000040, connection status changed
Is there any modification I need to do on base EVM? One board labeled BETA_0079 and the other labeled A2_0125