Other Parts Discussed in Thread: SYSBIOS
I'm attempting to build some DMAN3/ACPY3 code and I nned to define a heap in L1 memory. xdc is giving me the following error:
Error: memory name 'L1DSRAM' is not defined by the platform
How do I get xdc ro recognize the C674 internal memores?
My .cfg files:
DSPtasks_common.cfg.xs:
var Ipc = xdc.useModule('ti.sdo.ipc.Ipc');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
var Syslink = xdc.useModule ('ti.syslink.ipc.rtos.Syslink');
xdc.loadPackage ('ti.syslink.ipc.rtos');
if ( (Program.platform.$name != undefined) && (Program.platform.$name.match(/evmDA830/)) ) {
/* Ipc */
Ipc.sr0MemorySetup = true;
}
/* Ipc configuration */
if ( (Program.platform.$name != undefined) && (Program.platform.$name.match(/evm6472/)) ) {
/* Set host id */
Ipc.hostProcId = MultiProc.getIdMeta("CORE5");
Ipc.generateSlaveDataForHost = true;
}
else if ( (Program.platform.$name != undefined) && (Program.platform.$name.match(/evm6474/)) ) {
/* Set host id */
Ipc.hostProcId = MultiProc.getIdMeta("CORE2");
Ipc.generateSlaveDataForHost = true;
}
else {
/* Set host id */
Ipc.hostProcId = MultiProc.getIdMeta("HOST");
}
Ipc.procSync = Ipc.ProcSync_PAIR;
/* Set Shared Region variables by picking up the information from Platform
* memory map
*/
var sr0MemSection = Program.cpu.memoryMap['SR0'];
var SHAREDREG_0_MEM = sr0MemSection.base;
var SHAREDREG_0_MEMSIZE = sr0MemSection.len;
var SHAREDREG_0_ENTRYID = 0;
var SHAREDREG_0_OWNERPROCID = Ipc.hostProcId;
var sr1MemSection = Program.cpu.memoryMap['SR1'];
var SHAREDREG_1_MEM = sr1MemSection.base;
var SHAREDREG_1_MEMSIZE = sr1MemSection.len;
var SHAREDREG_1_ENTRYID = 1;
var SHAREDREG_1_OWNERPROCID = Ipc.hostProcId;
/*
* Need to define the shared region. The IPC modules use this
* to make portable pointers. All processors need to add this
* call with their base address of the shared memory region.
* If the processor cannot access the memory, do not add it.
*/
SharedRegion.setEntryMeta(SHAREDREG_0_ENTRYID,
{
base: SHAREDREG_0_MEM,
len: SHAREDREG_0_MEMSIZE,
ownerProcId: SHAREDREG_0_OWNERPROCID,
isValid: true,
name: "shared_region_0",
});
SharedRegion.setEntryMeta(SHAREDREG_1_ENTRYID,
{
base: SHAREDREG_1_MEM,
len: SHAREDREG_1_MEMSIZE,
ownerProcId: SHAREDREG_1_OWNERPROCID,
isValid: true,
name: "shared_region_1",
createHeap: true
});
/*
* Application constants that all three programs use.
*/
Program.global.MSGQ_NAME = "MSGQ_";
Program.global.HEAP_NAME = "HeapMemMP";
Program.global.HEAP_ALIGN = 128;
Program.global.HEAP_MSGSIZE = 128;
Program.global.HEAP_NUMMSGS = 10;
Program.global.HEAPID = 0;
DSPtasks_ti816x_dsp.cfg:
/* Set the BIOS timer frequency to 32KHz so as to match with the default timer
* frequency on Linux
*/
var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
Timer.intFreq.hi = 0;
Timer.intFreq.lo = 32768;
var System = xdc.useModule('xdc.runtime.System');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.setConfig("DSP", ["DSP", "VIDEO-M3", "VPSS-M3", "HOST"]);
/* Load common configuration needed for running all SysLink samples */
xdc.loadCapsule("DSPtasks_common.cfg.xs");
var Notify = xdc.useModule('ti.sdo.ipc.Notify');
var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Sem = xdc.useModule('ti.sysbios.knl.Semaphore');
var Memory = xdc.useModule('xdc.runtime.Memory');
Memory.defaultHeapSize = 0x8000;
Program.heap = 0x8000;
/* Configure some BIOS heaps */
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
heapMemParams.size = 0x4000;
heapMemParams.sectionName = ".L1D_HEAP";
/* Create L1DHEAP as global variables so it can be used in C code. */
Program.global.L1DHEAP = HeapMem.create(heapMemParams);
// Place heaps. L1DSRAM is defined in platform file
Program.sectMap[".L1D_HEAP"] = "L1DSRAM"; // L1DHEAP
//Program.sectMap[".EXTERNAL_HEAP"] = "DDR2"; // EXTERNALHEAP
Program.sectMap[".text"] = "DDR2";
/* Task that does the message passing */
var tsk1 = Task.create('&Preprocessing_taskFxn');
tsk1.instance.name = "Preprocessing_taskFxn";
tsk1.arg0 = MultiProc.getIdMeta ("HOST");
tsk1.stackSize = 0x1000;
/* DMAN3 stuff */
var DMAN3 = xdc.useModule('ti.sdo.fc.dman3.DMAN3');
DMAN3.heapInternal = "L1DHEAP";
DMAN3.heapExternal = "DDR2";
DMAN3.numQdmaChannels = 8;
DMAN3.paRamBaseIndex = 78;
DMAN3.numPaRamEntries = 48;
DMAN3.nullPaRamIndex = 127;
DMAN3.tccAllocationMaskH = 0xffffffff;
DMAN3.tccAllocationMaskL = 0x0;
DMAN3.numTccGroup = [4, 3, 2, 0, 0, 5];
DMAN3.numPaRamGroup = [4, 4, 2, 0, 0, 5];
DMAN3.qdmaChannels = [0, 1, 2, 3, 4, 5, 6, 7];
DMAN3.maxQdmaChannels = 8;
DMAN3.maxTCs = 2;
/* ACPY3 stuff */
//var ACPY3 = xdc.useModule('ti.sdo.fc.acpy3.ACPY3');
Lee Holeva