Hello,
I'm a bit confused on the combinations of possibilities with emulators vs. connectors vs. target board headers. My target board is physically small, I can only plan for 1 header for debug of the OMAP-L137. I think I will purchase the XDS100v2, maybe one that has a native 20-pin connector.
Is it possible to have only one on-board target header to debug both the DSP and ARM cores?
What header (14-pin, 20-pin CTI, ARM 20-pin) do I use in the target board schematics?
Will the XDS100v2 emulator need an adapter if debugging in DSP or ARM mode or can both cores be debugged simultaneously?
Best regards,
SC