This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 and UART communication

Hello,

 

I ma using C5515 Fingerprint development kit. I need to modify a demo application to use UART.

I am running C55XCSL-LOWPOWER-2.0.00.00 CSL Uart DMA example, by using XDS510USB JTAG and CCS 4.2

I get NO output on the HyperTerminal of windows when all the settings are correct (according to the CSL UART EXAMPLE DOCUMENTATION) that is coming with CSL.

The question is what can be wrong? I am setting the PLL tp 60 MHz by running script from CCS menu (after I connect to target and load the program)

Additional question that I have is there is no correspondance between the registers as described in C5515 UG and registers that are displayed in debug menu of C5515. Can u explain why is that?????

Regards