We recently bought a second TMDSEVLM138 OMAP-138 EVM and are unable to run the code we developed on our original OMAP-138 EVM. We are using the TMS320C6748 DSP SOM on both boards. The original EVM came with rev A of the SOM and the new EVM came with rev B of the SOM. The code crashes on the new board when I attempt to initialize the EMIFA interface to talk to a peripheral board that is plugged into it. When I remove this initialization code the rest of the code runs fine but of course I can’t talk to the peripheral. I have NOT updated any of the BSL or CSL libraries that I was using with the original EVM.
Thanks,