This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO Activation



Hello,

 

I am trying to toggle a GPIO pin:

For example, to toggle pin GP0[12] I set bit 12 in DIR01 (first) and then OUT_DATA01 or SET_DATA01 or CLR_DATA01 registers. The problem is that this works only for bank0. When I am trying to change GP4[0] - it changes the register but not changing the pin state. And so goes for all pins except bank0. Do I need to enable anything for other banks?

I am using OMAPL137EVM.

Regards

Arye