The migration guide does not stipulate a recompile. However, does the memory modification potentially cause an issue with binary compatibility?
This is a resurrection of a very old design and it is not feasible to do a recompile. However, it is expensive to roll the CCA and it is imperative that there is 100% confidence in the binary compatibility between the two device revisions.