hi,
i compiled gingerbread dsp, now i have three issues
1. CMEMK Error: CMEM phys_start (0x8c900000) overlaps kernel (0x80000000 -> 0x90000000)
is it ok if i make changes in init.omap3.rc as
insmod /system/ti-dsp/cmemk.ko "phys_start=0x90000000 phys_end=0x90800000 pools=20×4096,10×131072,2×1048576,1×5250000,4×829440,2×691200"
2. i am using kernel image downloaded from prebuilt tar, the kernel image built while building gingerbread gets stuck at "uncompressing kernel"
how do i find what is the problem
3. i have a touch screen which is basically used in cars, it has hdmi port, what boot script should i use for using this screen as a display
with best regards
parimal naigaonkar